2024-12-09 3:44 AM
Hello,
I recently upgraded my CubeMX to V6.12.1 from V6.6.1. All of a sudden, I have realised that when I generate code from the updated CubeMX, it removes my Post build command line from my IAR EWARM project.
Is there a new setting or such that I am missing that does not do that? Or is it a CubeMX problem?
I thank you in advance!
Makarand
2024-12-10 6:34 AM
Hello @Makarand
First let me thank you for posting.
1- In STM32CubeMX, ensure that the option "Backup previously generated files when re-generating" is checked. This setting can help preserve your previous configurations, including build steps, although it may not guarantee complete retention of custom commands.
2- Scripted Backup: Create a script that automatically saves your current post-build commands to a separate file before each code generation.
3- Check the project settings in IAR and ensure that the post-build commands are correctly configured under Project > Options > Build Actions > Post-build Command. Sometimes, reconfiguring these settings can help maintain them during regeneration.
THX
Ghofrane
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-12-24 4:25 AM
Hello,
Thank you for the solutions, however, it did not work. I was using 6.6.1 earlier where this problem was not there.
For solution 1 - Along with backing up the files, I also unchecked the "Delete previously generated files if not re generated" option, but that did not help either.
As for no. 3, I did check the configuration, and it looks okay when I add the post build command into it manually. However, on generating code from CubeMX, it is removed.
I can see that in the code generator, there is an option of user actions before and after code generation.
Is there any literature available on how to use this feature? Could something be done in this feature that prevents my project settings from changing?
I thank you in advance!
Makarand
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.