2022-01-31 11:07 AM
I have intermittent problems in STM32CubeIDE 1.8.0 opening a .ioc file. When I double click on the file in the Project Explorer, I get a progress bar titled "Loading IOC". When things are working well, as soon as that bar fills up, it is replaced with a progress bar titled "Completing IOC Load"; and when that fills up, the configuration screen is dsplayed.
Sometimes the IDE gets into a state where the first progress bar will fill up, but the second one never appears. Instead, the window hangs--I get a spinning cursor, and the Windows message "not responding". This lasts forever. If I force quit the IDE and retry, many times, eventually it starts working again.
How can I keep this from happening, and if it does happen, how can I reliably and quickly recover?
2022-02-01 4:38 AM
Hi,
How often does the error state happens? 1 in 10 attempts to open the ioc-file or more frequently?
I am wondering if it would be possible to copy the ioc-file and open it in CubeMX stand-alone to see if the same error occurs in MX stand-alone. That insight would indicate where we should start to have a deeper look (In MX or in the bridge/integration between MX and IDE)..
Are you able to share the ioc-file producing this issue? But maybe it only happens on your system...
Next time you encounter the issue could you immediately have a look in the workspace log-files and see if there are any exceptions that seem related (with related I mean "time stamp wise") to the error?
The log-files are in the folder $(workspace_dir)\.metadata\.
Post your findings please!
2022-02-01 5:55 AM
The latest CubeIDE versions seem to have a lot more unnecessary communicating with the ST servers than previous versions which seems to lead to this behavior if something goes slightly amiss. It's very annoying. If you load an IOC file, and all necessary libraries are already on your PC, the IDE shouldn't need to check for new versions or talk to ST servers at all, and yet it does.
2022-02-01 7:44 AM
@TDK Have you also experienced this hang? It would be helpful to know that it's not just the installation on my machine that is doing this (admittedly, I'm using W7, and the computer only has 8G RAM, so it's possible that it's a Windows or memory-related issue).
2022-02-01 7:49 AM
@mattias norlander It's hard to say how often this happens--I had it happen a few times in one day recently, after not encountering it for a number of days. Once it happens, though, it's stuck--many quits and restarts of the IDE don't fix it. I did in fact investigate the logfiles. The suspicious thing I noticed was a message to the effect (on IDE launch) that an instance of MX was already running. So I suspect that maybe there is an ophaned MX process or a leftover lockfile. If you could tell me the Windows process name for MX and/or the locations and names of any lockfiles that I might delete, that would be helpful. I have looked but so far haven't figured out either of those. Obvioulsy *something* is retaining some state to cause it to keep hanging after relaunching STM32CubeIDE.
2022-02-02 6:13 AM
Hypothesis: Maybe The CubeMX plug-in does not shutdown properly leaving an orphaned process. Maybe this could block you from opening the same, or another, ioc-file again.
I doubt that a restart of CubeIDE would solve that.
But rebooting the computer should clean out such process.
So, next time this happens could you try the following four step approach to see what works?
These could be some pointers as to how you can troubleshoot this.
It is a bit difficult to give guidance since I cannot re-produce your problems.
From the next release, CubeIDE will officially only support Win10 and later versions.
We will also drop support to any MacOS version previous to 10.15.
We have already seen some issues with Windows version which are end-of-life. Another factor is that we cannot claim support for OS versions that our underlying frameworks even officially support...
2022-02-02 7:59 AM
1) Restarting CubeIDE does not help--I've done that many times.
2) I did try CubeMX standalone a while back, and although my memory is not clear, I think that it worked but I still had the problem when I went back to CubeIDE.
3) Yesterday in fact I did try rebooting the computer, and in that instance it fixed the problem.
2022-02-02 8:31 AM
I think I have found the trigger for the issue. If I am duplicating a project, if I've copied and renamed the .ioc ifle, but don't edit it to update the two places that the project name appears inside, that causes the problem.
To answer your question 4), deleting .stm32cubemx and .stmcufinder does not help. And when I recreated the problem this way, this time rebooting the computer *did not* fix the problem. Also, opening the .ioc in the standalone MX did not fix the problem with the IDE MX, even if I "generate code" from the standalone MX.
Right now, it is in the state where it hangs if I try to open the .ioc file. When I launch the IDE, this is what appears in .metadata/.log:
--------------------------------------------------------------------------------------------------------------
!SESSION 2022-02-02 11:15:30.771 -----------------------------------------------
eclipse.buildId=Version 1.8.0
java.version=11.0.11
java.vendor=AdoptOpenJDK
BootLoader constants: OS=win32, ARCH=x86_64, WS=win32, NL=en_US
Command-line arguments: -os win32 -ws win32 -arch x86_64
!ENTRY com.st.stm32cube.ide.mcu.informationcenter 4 4 2022-02-02 11:15:35.724
!MESSAGE CubeMX plugin appears to be active, Log4j initialization might be too late.
!ENTRY com.st.stm32cube.ide.mcu.informationcenter 1 1 2022-02-02 11:15:35.794
!MESSAGE Log4j initialized with config file C:\Users\mschuman\STM32CubeIDE\workspace_1.8.0\.metadata\.log4j.xml
!ENTRY com.st.stm32cube.ide.mcu.ide 1 1 2022-02-02 11:15:41.981
!MESSAGE Started RMI Server, listening on port 41337
-------------------------------------------------------------------------------------------------------------------
So it must be looking at some lockfile or other indicator of status to tell it that there is an unfinished MX session out there. It should be possible to look at the code and see what prompts that logfile entry.....
2022-02-04 2:14 AM
Ok, not sufficient log level to catch anything.
Could you try to increase the log level?
If using CubeMX standalone:
Set the log4j,properties in .stm32cubemx folder
It is the line: log4j.rootLogger=*** which defines the level of log (INFO = standard, TRACE = INFO + additional information)
If using CubeMX integrated in CubeIDE:
In the file /.metadata/.log4j.xml
Modify the line :
param name="Threshold" value="INFO"/
with
param name="Threshold" value="TRACE"/
2023-10-02 7:38 PM
Ran into this issue on macOS. Restarting the OS (NOT just ide) solved issue.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.