STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1756 Views
  • 0 replies
  • 2 kudos

Resolved! Potentially wrong initial value of SCB->VTOR

Good day,after troubleshooting some issues related to a bootloader, I have figured out that the address of the interrupt vector table (SCB->VTOR) is defined in a hard-coded, non linker aware way as "SCB->VTOR = FLASH_BASE | VECT_TAB_OFFSET". This mea...

dfrejek by Associate III
  • 5429 Views
  • 7 replies
  • 8 kudos

STM32CubeMX 6.13.0 cannot be installed in Win11

Hello everyoneI changed my PC to one with Win11 and I cannot install the CubeMX.After I downloaded and started the setup, the extracting windows appears and after the splash screen remains opened for few second and then close.Nothing else, I have a p...

Resolved! stm32cubemx utilities folder is missing

Hi!I have created a few projects to practice working with the STM32H series. Then, I selected SPI or I2C and used GPDMA linked-list. According to many tutorials, I should have gone to the utilities folder to configure GPDMA, but such a folder did not...

jkarczew by Associate
  • 4875 Views
  • 3 replies
  • 0 kudos

Resolved! Possible Bug in STM32CubeMX v6.13.0

Hi, I am using the STM32G0B1CBTx on the STM32CubeMX and setting the I2C1 for SMBus-two-wire-Interface. I want to disable the timeouts but I noticed that when I do so, the clock timeout enable (bit 15 of I2C_TIMEOUTR register) is still high. Looking a...

DDeba1_0-1739962440422.png
DDeba.1 by Associate III
  • 1002 Views
  • 1 replies
  • 2 kudos

Resolved! Code generation problem for FileX

Hello,I am using STM32H730ZBT6 with STM32 CubeMX V6.12.1 (I am not using the newest version because of the problem related in topic Downgrade STM32CubeProgrammer in STM32CubeIDE. I dont' know exactly if CubeMX would reproduce the problem, but for the...

ego by Associate III
  • 3781 Views
  • 4 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.