STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1756 Views
  • 0 replies
  • 2 kudos

FreeRTOS SysTick_Handler missing

Moved from MPUs forum; STM32F072 is an MCU - not an MPU.Hi,I've just started a new project for a STM32F072 chip using STM32CubeIDE 1.17.0.When adding FreeRTOS support to my project, the program hangs soon after osKernelStart() is called.I had hard ti...

DrPiWork by Associate II
  • 2716 Views
  • 4 replies
  • 1 kudos

Resolved! Inconsistent pin numbering

Hi,We are working on a board with the STM32H7S7Z8J6 in a BG144 package. We use cubemx to create the correct pinout for this part, but we see the datasheet has different pinout then the CubeMX tool. Is this a bug in CubeMX?   

leddel32_1-1739833837502.png leddel32_2-1739833869608.png
leddel32 by Associate II
  • 1088 Views
  • 2 replies
  • 0 kudos

CubeMX UI is messed up (again, again and again...)

Despite referring to the STM32F0 label (can't this forum have a simple one labeled as a general problem for STM32CubeMX???) the problem exists for ALL situations and MCU's where you simply start working with the STM32CubeMX.Since several years ago, s...

[BUG] CubeMX switch off JTAG and SWD

Posted on October 29, 2017 at 01:12Hi all,I would like to report a bug of CubeMX.I did generated simple project for STM32F103VEx.  Project if fairly simple just uses USB in CDC mode.I did generate similar project for same processor but only SPI3 usi...

rafal23 by Associate II
  • 6716 Views
  • 8 replies
  • 4 kudos

Resolved! STM32F103: Option to assign pins to core M3 in CubeMX

Hello,When generating code via CubeMX, the main code does not contain the configuration for the GPIO pins I need to be using.I have checked other solutions and seen that the pins need to be assigned to the core (in this case it would be the M3). The ...

XPChi by Associate II
  • 2518 Views
  • 6 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.