STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1756 Views
  • 0 replies
  • 2 kudos

CPU caches checkboxes blocked

 STM32H7 SeriesI have enabled generation of linker script (need to redefine memory layout).There is no possibility to change  state of checkboxes of both CPU caches if this generation has been enabled.The state of the checkboxes may be on or off, but...

trzeci by Associate III
  • 608 Views
  • 0 replies
  • 0 kudos

Resolved! CubeMX CAD models mixing LQFP144 and 208pinouts

Trying to export LQFP144 pinout to Altium CAD models with cubeMX.  But CubeMX is trying add pin #204 #202 #158, etc, on symbol for an L471 micro that doesn't even come in packages  bigger than 144 pins.  Altium chokes on this symbol, I imagine that's...

Screenshot 2024-10-21 180625.png
DixonDon by Associate II
  • 1448 Views
  • 2 replies
  • 0 kudos

Resolved! STM32H725 SMPS issue

I am having and issue with a STM32H725RGV6.After powering my board, I can see the SMPS output at 1.36V, which I have connected to the VCAP inputs.I can also connect to the µC using the STM32CubeProgrammer.However, after flashing a simple firmware, th...

STM32H725RGV6 power.png
BenUtzer by Associate
  • 3535 Views
  • 3 replies
  • 2 kudos

Resolved! stm32cubeMX bug???

Hello,I am now using STM32CubeMX to config STM32G030F6P6, I want to use TIM14 to capture pulse, so I configged to Input Capture direct mode, which is obviously input port, but GPIO setting becomes GPIO output Low. is this a stm32cubeMX bug?please con...

dqsh06_0-1729747045042.png
dqsh06 by Senior
  • 3139 Views
  • 6 replies
  • 1 kudos

Resolved! Where in CubeMX can I check the Wait States?

Hi,I am using the STM32U5G9VJT6Q and in CubeMX I configured the clock to the full 160MHz for all busses including the core (first screenshot). According to the documentation for 160MHz I need to set 4 Wait States for those speeds and VCORE voltage ne...

Ricko_0-1741045992307.png Ricko_1-1741046086361.png
Ricko by Senior III
  • 1193 Views
  • 2 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.