2025-10-14 7:31 AM - last edited on 2025-10-14 7:56 AM by Andrew Neil
Defining the underlying type of an enumeration has been a difficult task until C23 added the feature. Previously different compilers used different methods and results could vary unexpectedly.
As seen in the image below, STM32CubeIDE v 1.19.0 can recognize this C23 feature and flag mistakes, such as the out-of-range value 0x101 for the 8-bit enum.
As seen in the gcc output below, the mistake is caught by gcc:
This is all as it should be. The problem is when I remove the fake out-of-range command, gcc works as expected but STM32CubeIDE flags a syntax error:
The build finished with no errors or warnings so gcc 13 understands at least this part of the C23 standard.
Is there a configuration within STM32CubeIDE to prevent displaying a Syntax error for code the compiler understands?
PS
I checked the generated assembly and it appears that the correct 8-bit code (ldrb) is being generated:
2025-10-17 2:15 AM
@Ozone wrote:I came across this issue with most of the Eclipse-based IDE I used.
Indeed - it is an Eclipse thing, not specific to CubeIDE.
But it's not unique to Eclipse; eg, the old Atmel Studio (MSVS-based) also did it.
I wonder if VSCode also does it ... ?
2025-10-17 2:56 AM
Exactly my point. Nothing to do with the compiler.
2025-10-20 3:57 AM
OK so we all agree that it has nothing to do with the selected toolchain, but is the Eclipse Language Server. But does anyone know a solution how to teach the Eclipse code highlighter the new C standard?
2025-10-20 4:13 AM - edited 2025-10-20 4:14 AM
I wouldn't! Although a comma in that case is digested by the toolchain, it is syntactically incorrect. This is rather like JSON which some lazy coders scatter with commas at the end of a list only to find that some JSON parsers don't mind and others fall over in a heap.
So rather than modifying the tool to mask a trivially fixed coding error, why not fix that error?
Bear in mind that compilers evolve forever and the next version may indeed choke on that comma.
I think that the language settings in Eclipse can be edited if you really want to modify the tool to mask this issue.
2025-10-20 4:39 AM - edited 2025-10-20 4:44 AM
@bramble wrote:it is syntactically incorrect.
Is it, though?
https://stackoverflow.com/questions/792753/is-the-last-comma-in-c-enum-required
PS:
Even if it is, the question remains valid as there are other issues where the Eclipse parsing gets it wrong; eg:
C23 syntax highlighting in STM32CubeIDE (e.g. constexpr)
CubeIDE incorrectly flags __attribute__((fallthrough)) as syntax error - which isn't even C23
2025-10-20 4:40 AM
@A.D. wrote:does anyone know a solution how to teach the Eclipse code highlighter the new C standard?
Does this help ?
2025-10-20 8:48 AM
No. Changing the language mappings didn't help with the Eclipse syntax highlighting not liking the storage specifier in the enumeration definition.
typedef enum SSP_CMDS_E : unsigned char
{
CMD_ID_REQ = 0x41, // ID Request
CMD_EXT_ID_REQ = 0x42 // Extended ID Request
} SSP_CMDS_E;It's either an Eclipse issue or an STM32CubeIDE issue. Not actually a bug since STM32CubeIDE doesn't claim to support C23 syntax. If this enumeration wasn't part of an 'over-the-wire' communications definition, I would just use a #define to avoid the issue.
At this point it's important to remember the job isn't to find a better way to shoot the alligators; the job is to drain the swamp.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.