2026-01-28 7:49 AM - edited 2026-01-28 7:52 AM
Extension 3.7.0
st-arm-clang 19.1.6+st.10
Hello,
I am using CubeIDE für VSCode.
I write programs for the STM32F756ZGTx. I have set ST Arm Clang as the compiler in CubeMX. Redirecting the output (printf()) via the serial debug interface is possible without any problems. When I try to output float or double values with printf(), I get some weird results.
printf() with integer float/double yields correct results for integer float/double wrong
printf() with float/double integer always leads to incorrect results
I repeated the experiment for double variables. The same problem occurs here as well.
#include "main.h"
#include <stdio.h>
extern UART_HandleTypeDef huart3;
double floatVar = 1.1f;
void mainThread(void)
{
printf("\r\n\nHello from Nucleo F756 - float Test\r\n"
"-----------------------------------\r\n");
for(;;){
printf("Float value: %f - Integer %u\r\n", floatVar, (unsigned int) floatVar);
printf("Integer %8u - Float value: %f\r\n", (unsigned int) floatVar, floatVar);
HAL_Delay(500);
floatVar += 1.0f;
}
}
int __io_putchar(int ch) {
HAL_UART_Transmit(&huart3, (uint8_t*) &ch, 1, 100);
return ch;
}
Variable type float
Hello from Nucleo F756 - float Test
-----------------------------------
Float value: 1.887500 - Integer 2684354560
Integer 1 - Float value: -0.000000
Float value: 2.012500 - Integer 3221225472
Integer 2 - Float value: -2.000000
Float value: 2.137500 - Integer 3221225472
Integer 3 - Float value: -2.000000
Float value: 2.256250 - Integer 1610612736
Integer 4 - Float value: 36893490000000000000.000000
Float value: 2.318750 - Integer 1610612736
Integer 5 - Float value: 36893490000000000000.000000
Float value: 2.381250 - Integer 1610612736
Integer 6 - Float value: 36893490000000000000.000000
Float value: 2.443750 - Integer 1610612736
Integer 7 - Float value: 36893490000000000000.000000
Variable type double
Hello from Nucleo F756 - float Test
-----------------------------------
Float value: 0.000000 - Integer 2684354560
Integer 1 - Float value: -0.000000
Float value: 0.000000 - Integer 3489660928
Integer 2 - Float value: -8589935000.000000
Float value: 0.000000 - Integer 3489660928
Integer 3 - Float value: -8589935000.000000
Float value: 0.000000 - Integer 1744830464
Integer 4 - Float value: 2417851600000000000000000.000000
Float value: 0.000000 - Integer 1744830464
Integer 5 - Float value: 2417851600000000000000000.000000
Float value: 0.000000 - Integer 1744830464
Integer 6 - Float value: 2417851600000000000000000.000000
Float value: 0.000000 - Integer 1744830464
Integer Please find enclosed the project.
What am I doing wrong? Is a linker or compiler option missing?
Thanks
Solved! Go to Solution.
2026-02-02 6:30 AM
I found a solution for the correct output. To do this, I added a line to starm-clang.cmake.
set(CMAKE_EXE_LINKER_FLAGS "${CMAKE_EXE_LINKER_FLAGS} -Wl,--defsym=vfprintf=__d_vfprintf -Wl,--defsym=vfscanf=__d_vfscanf") Here again in the context of the file
if (STARM_TOOLCHAIN_CONFIG STREQUAL "STARM_HYBRID")
set(CMAKE_EXE_LINKER_FLAGS "${CMAKE_EXE_LINKER_FLAGS} --gcc-specs=nano.specs")
set(TOOLCHAIN_LINK_LIBRARIES "m")
elseif(STARM_TOOLCHAIN_CONFIG STREQUAL "STARM_NEWLIB")
set(CMAKE_EXE_LINKER_FLAGS "${CMAKE_EXE_LINKER_FLAGS} -lcrt0-nosys")
elseif(STARM_TOOLCHAIN_CONFIG STREQUAL "STARM_PICOLIBC")
# added line to enable float support in printf/scanf
set(CMAKE_EXE_LINKER_FLAGS "${CMAKE_EXE_LINKER_FLAGS} -Wl,--defsym=vfprintf=__d_vfprintf -Wl,--defsym=vfscanf=__d_vfscanf") #<<<<
set(CMAKE_EXE_LINKER_FLAGS "${CMAKE_EXE_LINKER_FLAGS} -lcrt0-hosted -z norelro")After these changes, I can output both float and double values correctly. The combination with integer and float/double also works.
I would be very grateful if someone could tell me whether this is the approach planned by ST.
Thanks
2026-02-02 6:30 AM
I found a solution for the correct output. To do this, I added a line to starm-clang.cmake.
set(CMAKE_EXE_LINKER_FLAGS "${CMAKE_EXE_LINKER_FLAGS} -Wl,--defsym=vfprintf=__d_vfprintf -Wl,--defsym=vfscanf=__d_vfscanf") Here again in the context of the file
if (STARM_TOOLCHAIN_CONFIG STREQUAL "STARM_HYBRID")
set(CMAKE_EXE_LINKER_FLAGS "${CMAKE_EXE_LINKER_FLAGS} --gcc-specs=nano.specs")
set(TOOLCHAIN_LINK_LIBRARIES "m")
elseif(STARM_TOOLCHAIN_CONFIG STREQUAL "STARM_NEWLIB")
set(CMAKE_EXE_LINKER_FLAGS "${CMAKE_EXE_LINKER_FLAGS} -lcrt0-nosys")
elseif(STARM_TOOLCHAIN_CONFIG STREQUAL "STARM_PICOLIBC")
# added line to enable float support in printf/scanf
set(CMAKE_EXE_LINKER_FLAGS "${CMAKE_EXE_LINKER_FLAGS} -Wl,--defsym=vfprintf=__d_vfprintf -Wl,--defsym=vfscanf=__d_vfscanf") #<<<<
set(CMAKE_EXE_LINKER_FLAGS "${CMAKE_EXE_LINKER_FLAGS} -lcrt0-hosted -z norelro")After these changes, I can output both float and double values correctly. The combination with integer and float/double also works.
I would be very grateful if someone could tell me whether this is the approach planned by ST.
Thanks
2026-02-02 9:28 AM
This is an issue of the newlib nano or pico you are using. The don't support float formats by default. but supply a weak symbol which you may request linking like:
target_link_options(app PRIVATE
-specs=nano.specs
-Wl,-u,_printf_float
-lc
-lnosys
)or
clang --target=arm-none-eabi -mcpu=cortex-m4 -mthumb \
-ffreestanding -nostdlib -nostartfiles \
-I/path/to/picolibc/include \
main.c \
-L/path/to/picolibc/lib \
-lc -lm \
-Wl,-u,__printf_float \
-o out.elfHaven't used it with clang (yet?), but with gcc.
2026-02-18 1:35 AM
Sorry for the late reply. I tested it again. In my test program, -Wl,-u,__printf_float does not work for picolibc.
2026-02-18 1:38 AM
Alternatively, the following entry can also be made in CMakeLists.txt.
target_link_options(${CMAKE_PROJECT_NAME} PRIVATE
# Add user defined linker options
"-Wl,--defsym=vfprintf=__d_vfprintf"
"-Wl,--defsym=vfscanf=__d_vfscanf"
)
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.