STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1703 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 638 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

When building a C++ STM32 Project, how do I associate the .hpp file extension with combined header and source templates and Class files?

In my regular C++ work, I use the BOOST library, and I've taken to using their .hpp style that combines header declarations and source definitions in one file for most of my C++ work. I try to not use separate .h and .cpp files any more, whether it i...

DWild.1 by Associate II
  • 2416 Views
  • 2 replies
  • 0 kudos

Resolved! When copying a STM32 Project to a new C/C++ Managed Build Project, I am encountering header file location errors because I don't know how to duplicate the auto-generated project links under the master {project} Includes "directory."

It has the auto-generated plugin include "links", but I am missing the following.{project}/Core/Inc{project}/Drivers/CMSIS/Device/ST/STM32G4xx/Include{project}/Drivers/CMSIS/Include{project}/Drivers/STM32G4xx_HAL_Driver/Inc{project}/Drivers/STM32G4xx...

DWild.1 by Associate II
  • 3625 Views
  • 4 replies
  • 0 kudos

Resolved! Switching from Debug to Release mode - how do I push firmware to target (beginner question, am I doing something wrong?)

I am beginner with STM32CubeIDE 1.8.0 and am having trouble delivering release mode firmware to the attached target (STM32F0Discovery module, which is otherwise working well.)I am now experimenting with switching from Debug (the default configuration...

wb0gaz by Senior
  • 14305 Views
  • 8 replies
  • 0 kudos

Resolved! Dual bootloader - how to?

Hi everyone!I have to implement a dual bootloader system on different stm32 microcontrollers in STM32cube ide, and I have some questions…The idea is the following:There is a “pre-bootloader�? at the beginning of the flash. When it starts, it gets som...

Resolved! How to add preprocessor symbol in STM32Cube IDE

#error "Define according the used Cortex core ARM_MATH_CM7, ARM_MATH_CM4, ARM_MATH_CM3, ARM_MATH_CM0PLUS or ARM_MATH_CM0"Based from this Topic https://community.st.com/s/question/0D50X00009XkXPtSAN/need-help-in-dsp-library-for-keil- The problem is so...

How do I configure an Rx only UART interface in cubeide?...

I dont want to 'waste' the pins on the Tx line as this will not be used (the datastream is one way from an RC receiver into the STM32) - This isnt a case of it being a half-duplex etc.I can set the direction of data to be receive only in the advanced...

JHoun.1 by Associate III
  • 3863 Views
  • 5 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.