STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1703 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 638 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Resolved! I have an error of "multiple definition of `ProcessChar' I have the function ProcessChar() in two source files. There are no header files or prototypes that should make these functions global.

This is a project created with STM32CubeMX and then coding in the STM32CubeIDE environment.The error is in the linking process, but wondering why the linker should believe this function is defined twice by default. I had reason to believe these shoul...

Mike xx by Associate III
  • 3554 Views
  • 4 replies
  • 0 kudos

Resolved! How to link library (.c and .h file) in CubeIDE?

Hello, I'm new in STM32CubeIDE.I want to create my library to use in my C/C++ project.My library includes 2 files (.c and .h) but I don't know how to linking them in CubeIDE.Anyone can help me? Many thanks,Hieu

Resolved! Migration from TrueStudio to STM32CubeIDE, "Fail create backup of project files before conversion." No other message. How to debug this?

Hello,We have a long-lived project that we develop in Atollic TrueStudio. It contains 4 nested projects; two C/C++ projects, and another two Eclipse projects for web development.I have tried to import these projects using the "Import/General/Import ...

PDools by Associate II
  • 5664 Views
  • 10 replies
  • 0 kudos

Resolved! How to still listen to UART1 or any other UART using 115200 baud rate in STOP mode ? (STM32L053 has an LSE of 32.768kHz and LSI of 37kHz)

I want to listen to UART (using receive interrupt) at a baud rate of 115200 while in stop mode and retain the received characters (which are stored in a buffer) after I wake up from STOP mode using the RTC. Is that possible?If so, how do I implement ...

AV.9 by Associate II
  • 2067 Views
  • 1 replies
  • 0 kudos

Installer for CubeIDE broken for package L4 V1.17.1?

Do anyone experience the same problem?I tried to install the firmware package for STM32-L4 micros.I chose V.1.17.1. Installation started to download a file stm32cube_fw_V1170.zip despite the fact, that I chose V1.17.1Later it complained about a folde...

0693W00000JOReWQAX.png 0693W00000JORftQAH.png

Resolved! GDBServer not running under Debian

When I try to run the gdbserver included with cubeIDE the program reports it's missing "_Z19STLink_GetLibApiVerv", as in it cannot lookup the symbol within the binary.I encountered this error with both 1.7.0 and 1.8.0.I'm not sure if my LD_LIB_PATH i...

AHigg.2 by Associate
  • 2239 Views
  • 3 replies
  • 0 kudos

Resolved! How to add a third-party library to stm32cubeide permanently?

I have written multiple .c and .h files as libraries. Right now I have to add them to the core folder manually for each and every project I make. Is there any way that I can put these libraries in the main include folder of stm32cubeide, so I just ne...

AKari.3 by Associate
  • 2364 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.