STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1703 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 638 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Beginner with STM32CubeIDE (1.8.0) installed (on Windows) and STM32F0DISCOVERY, want open/import "blink the LED" type example.

Completed firmware update at Help > ST-LINK Upgrade, so STM32CubeIDE is communicating with STM32F0DISCOVERY module.Now trying find a most-basic example (for example, the firmware present in the STM32F0DISCOVERY board would be a good start - blink LED...

wb0gaz by Senior
  • 2349 Views
  • 3 replies
  • 0 kudos

why custom loader file work fail

I try to make a custom external loader on "STM32H750B-DK" EVM.The custom external loader file can not work fine. "H750_External_Boot_V2.zip" is my make external loader file project, but I do knowmy custom external loader file why can not to work fine...

0693W00000JNAzuQAH.png 0693W00000JNB04QAH.png 0693W00000JNB0TQAX.png
YCF.1 by Associate III
  • 774 Views
  • 0 replies
  • 0 kudos

Resolved! STM32CubeIDE vs Keil µVision generated code size

Hello,I used to generate code from STM32CubeMX then edit, compile and flash to board with Keil µVision (default config). Recently, I followed bootloader tutorial that uses STM32CubeIDE and I must admit it's nice but for exact same source code, the ge...

Thomas LB by Associate III
  • 3642 Views
  • 4 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.