STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1703 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 638 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Exceptions in logs.

Following exceptions occur very often while using STM32CubeIDE:Message: Unhandled event loop exceptionjava.lang.NullPointerException at org.eclipse.cdt.internal.ui.buildconsole.BuildConsoleManager.lambda$1(BuildConsoleManager.java:412) at org.eclipse...

HTD by Senior III
  • 1048 Views
  • 0 replies
  • 0 kudos

Resolved! How to create project in CubeIDE for STM32H750B-DK board that will use internal (128KB) and qspi external flash for code - any examples or docs ?

Hello,I'd like to learn more and understand how to create project that will work with code in internal and (or only in) external Flash ?Examples in CubeH7 seems to be set to address of external Flash memory.Thanks in advance,regards.

bully by Senior
  • 1799 Views
  • 1 replies
  • 0 kudos

Resolved! STM32G0 bought with level 2 protection

Hi all, I'm new to this STM32 community.I have a small problem: I bought some STM32G0P0.. for my project, also making the PCB and the rest. But after soldering the various components, I try to program one and see that the level 2 protection is active...

0693W00000WIxGqQAL.png 0693W00000WIxHFQA1.png

How to debug main.cpp imported from mbed and visualize the contents of variables

�?�在�?�ステータス:I次�?�図�?�示�?�よ�?��?��?2 �?��?�ヘッダー ファイル�?� 1 �?��?� cpp ファイルを mbed �?�ら Core/Src �?�イン�?ート�?��?��?��?�。�?��?��?��?cppコードをコンパイル�?�る�?��?無数�?�エラー�?�発生�?��?��?�。知り�?��?��?��?�ヘッダーファイル�?��?�る場�?��?�?��?��?�れ�?�デ�?ッグ�?��??�?��?��?�?エラーを解決�?�る...

0693W00000Y6uMkQAJ.png 0693W00000Y6uMuQAJ.png 0693W00000Y6uNOQAZ.png
hsanr.1 by Associate II
  • 2445 Views
  • 3 replies
  • 0 kudos

I am trying to run some applications on STM32 through the STMCubeIDE. Just wanted to know if there is any API which can be used inorder to perform the same functions using CLI.

The overview of the workflow is as follows: Open the STMCubeIDE -> Open new Project -> elect the directory -> Build -> debug -> buildSo I am looking for a python library/API which can be used to perform the same function through Automation. The UI au...

VNaga.2 by Associate II
  • 4725 Views
  • 9 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.