STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1703 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 638 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Resolved! Clear Pinouts Function in STM32CubeID

Hello, I am new and I am starting to program the STM32 with the help of the Nucleo 144 board and STM32CubeID.If I do a Clear Pinouts from the IDE, all the micro pins turn gray. I understand that they lose their configuration, including the TCK and TM...

Jgarc.11 by Associate II
  • 4568 Views
  • 4 replies
  • 0 kudos

Issue with running L152 discovery board + example.

I flashed the STM32 L152 discovery board with Cube IDE. I assume that if I run/debug the project with board plugged in, it will automatically upload the firmware. However, it shows as File download completeTime elapsed during download operation: 00:0...

ESHEE.1 by Associate
  • 1500 Views
  • 1 replies
  • 0 kudos

Resolved! How can I calculate an approximate IWDG window ?

Development Board: Nucleo-L476RG.IDE version: STM Cube IDE 1.11.0For the system watchdog timer, there's an equation(attached.) Is there an equivalent equation for the IWDG ?Any suggestions would be appreciated.Thanks

mm.51 by Associate II
  • 5715 Views
  • 1 replies
  • 1 kudos

Autocomplete (Content Assist) with any character

The current IDE does not open autocomplete automatically which is frustrating moving from "IntelliJ IDEA" to "Eclipse" it's not like the IDE is incapable of this, this is a working feature allowed for JAVA code just not C/C++In Cube IDE,Eclipse > Pre...

HBegn.2 by Associate
  • 4388 Views
  • 1 replies
  • 1 kudos

Resolved! How do I enable SWV in my STM32Cube ide?

I am trying to use SWV viewer but in Debugger option, there is no SWV options available. Is it because of some faulty pin configuration? Because i ran a blink led program and it's working fine. Just the SWV, i cannot enable.

0693W00000Y7ZK6QAN.png
RShre.2 by Associate III
  • 7769 Views
  • 3 replies
  • 0 kudos

Resolved! Wrong stack pointer for STM32F103C8

When creating a new project in the STM32CubeIDE for a STM32F103C8 (64k flash, 20k ram), the generated linker-script contains:/* Highest address of the user mode stack */ _estack = ORIGIN(RAM) + (LENGTH(RAM) / 2); /* end of "RAM" Ram type memory */   ...

ASeib.2 by Associate II
  • 2959 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.