2023-01-04 9:22 AM
Development Board: Nucleo-L476RG.
IDE version: STM Cube IDE 1.11.0
I have implemented this
"Configuring the IWDG when the window option is disabled When the window option it is not used, the IWDG can be configured as follows:
1. Enable the IWDG by writing 0x0000 CCCC in the IWDG key register (IWDG_KR).
2. Enable register access by writing 0x0000 5555 in the IWDG key register (IWDG_KR).
3. Write the prescaler by programming the IWDG prescaler register (IWDG_PR) from 0 to 7.
4. Write the IWDG reload register (IWDG_RLR).
5. Wait for the registers to be updated (IWDG_SR = 0x0000 0000).
6. Refresh the counter value with IWDG_RLR (IWDG_KR = 0x0000 AAAA)."
I'm not sure as to how I can validate that my processor is resetting.
Any suggestions would be appreciated.
Thanks
Solved! Go to Solution.
2023-01-05 12:30 AM
> how I can validate that my processor is resetting
Start the IWDG and don't refresh it (just spin) for a few minutes.
The MCU should reset. In your main() function read the reset reason and check that it is because of IWDG:
uint32_t reset_flags = RCC->CSR;
if (reset_flags & RCC_CSR_IWDGRSTF) {
// This was IWDG
}
else if (reset_flags & RCC_CSR_WWDGRSTF) {
// This was WWDG
}
else if (reset_flags & RCC_CSR_SFTRSTF) {
// Software reset (NVIC_SystemReset or by debugger)
}
2023-01-04 9:31 AM
In main code start read reset flags and clear it.
2023-01-05 12:30 AM
> how I can validate that my processor is resetting
Start the IWDG and don't refresh it (just spin) for a few minutes.
The MCU should reset. In your main() function read the reset reason and check that it is because of IWDG:
uint32_t reset_flags = RCC->CSR;
if (reset_flags & RCC_CSR_IWDGRSTF) {
// This was IWDG
}
else if (reset_flags & RCC_CSR_WWDGRSTF) {
// This was WWDG
}
else if (reset_flags & RCC_CSR_SFTRSTF) {
// Software reset (NVIC_SystemReset or by debugger)
}
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.