STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1703 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 638 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Hardfault when accessing a global variable in a position independent program compiled with -fPIE

Hello board,I seek to implement a position independent firmware to achieve a dual slot fota strategy:The application firmware can be saved into one among two possible memory areas, the firmware does not know at compile time where it will be stored so...

debugging.jpg debugging 2.jpg

RF Communication with 2 STM32F407VG disc1 boards.

Hi guys!I'm currently in charge of a project based on the RF transaction. My project is based to develop a system that have the ability to communicate with the RF transceiver, first I chose the AS4432SMD developed with the SI4432 transceiver and I tr...

Zayoud by Associate III
  • 4401 Views
  • 3 replies
  • 0 kudos

is it possible to download the code without reset pin

Hi everyone,so i am working on STM32C011F6P6and i found i can only download code with reset pin connectedotherwise this error will come upbut i want to have gpio function on reset pinis it possible to not use reset pin and get the download thing done...

stm32_download_issue.jpg

evspin32f0601s1 code not building

 I am trying to build the code on STM32CUBE IDE Version: 1.13.0. This code for evspin32f0601s1 is generated by CubeMX.It is throwing up 3 errors as below:C:\Program Files\STMicroelectronics\STM32CubeIDE_1.13.0\STM32CubeIDE\plugins\com.st.stm32cube.id...

Amit G by Associate II
  • 5228 Views
  • 8 replies
  • 0 kudos

PROBLEM TO PORTING X-CUBE-CRYPTOLIB ON MY PROJECT

Hello everyone. I create a project with X-CUBE-FREERTOS with STM32CUBEMX and I load it in STM32CUBEIDE,afterwards I had download the package X-CUBE-CRYPTOLIB 4.1.0 and import it follows the istructions here https://wiki.stmicroelectronics.cn/stm32mcu...

rdl by Associate III
  • 5216 Views
  • 4 replies
  • 0 kudos

STM32Cube IDE "Run" works, "Debug" doesn´t

Hello everyone,I have a problem with my STM32f746g_Disco. When I started a project, I could hit the "Debug" button and everything worked fine.Now it uploads everything and the Screen just shows a static noise (like on an old TV). When I use the "Run"...

JStei.6 by Associate III
  • 7382 Views
  • 6 replies
  • 1 kudos

Compile error with InfraredPD_CM0P_wc32_ot.a library.

Hello!We have a project for STHS34PF80TR IR sensor.We are setting the library "InfraredPD_CM0P_wc32_ot.a" in project options, but following compiler error is generated:c:\st\stm32cubeide_1.11.2\stm32cubeide\plugins\com.st.stm32cube.ide.mcu.externalto...

LMehm by Associate III
  • 1768 Views
  • 2 replies
  • 0 kudos

stm32cubeide crashes on ubuntu after upgrade

Hello,I upgraded my IDE to 1.13.0 yesterday on Ubuntu 22.04 and now it crashes just after startup. I can see no error message on the console.Even the previous version 1.12.x now crash.What information do you need from my system to pass on?Kind regard...

PGild.1 by Associate III
  • 1516 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.