STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1703 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 638 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

STM32CubeIDE examples for Nucleo-F446ZE

I know I can load Nucleo-F446ZE examples from the STM32CubeIDE, but what I find really annoying is the the examples provided are made in SW4STM32 IDE .To me it is very strange that while STM is promoting their STM32CubeIDE, I have to learn the SW4STM...

Copeland by Associate II
  • 1521 Views
  • 1 replies
  • 0 kudos

Resolved! how to change output pin to pwm pin

hello guys i am new to stm,i am using stm32103 and stmcubeide ,my question is very basic ,i know how to initialize a pin as an output pin or as a pwmpin but i donot know that how to change an output pin into a pwmoutput pin and then again convert tha...

ahmash by Associate III
  • 3739 Views
  • 2 replies
  • 2 kudos

Resolved! PH3-BOOT0

Hi,I am using STM32U585RIT6 MCU & I planned to flash the firmware through SWD and onboard debugger module (STLINK-V3MODS) through VCP.I am having confusion in configuring the PH3-BOOT0 pin.Should I connect it to 5V or GND.Or shall I make it No connec...

mkm by Associate
  • 1860 Views
  • 1 replies
  • 1 kudos

Error in initializing ST-Link

Hello Sir,     I'm new to this STM 32 environment. I'm using Nucleo F429ZI board when I try to debug the board it shows the following error."Error in final launch sequence:Failed to execute MI command:target remote localhost:61234Error message from d...

MA by Associate II
  • 2971 Views
  • 5 replies
  • 0 kudos

B-L475EIOT01A1 Example Code

Hi,New to STM32 tooling and am trying to find example source code for the B-L475E-IOT01A1 board.Nothing seems to pop up on the Example Selector of the Target Selector window and there doesn't seem to be any downloads for examples from the product pag...

Resolved! FreeRTOS: Only one of two tasks are occurring

Hello,I am utilizing a FreeRTOS system on the STM32H725AGI6 in my software with two purposes:- Run a task that handles the TouchGFX process to operate an LCD display- Run a task that handles a BLE process (Which utilizes theBlueNRG-M0A)I have tested ...

KMew_7-1691714181441.png KMew_0-1691713695694.png KMew_1-1691713715092.png KMew_2-1691713738276.png
KMew by Senior III
  • 5927 Views
  • 2 replies
  • 1 kudos

STM32CubeIDE DEBUG - save SFR values (state snapshot)

Dear All,I would like to make a snapshot of CPU registers (SFRs) when a program is paused.Ideally the snapshot would be a textfile.Does anyone know whether this is possible in CubeIDE or via some other tool?Thank youMatej

MMici.1 by Associate III
  • 6434 Views
  • 12 replies
  • 8 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.