STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1703 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 638 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

STM32F439ZI ETHERNET TCP CONNECTION

Hi,I am using stm32f439zi eval board for TCP communication. I can ping the board from host. It shows TCP connection error in Hercules utility. I am using port number 7 to listen to server. I am not sure whether I am using correct port number for the ...

arun27 by Associate II
  • 1082 Views
  • 1 replies
  • 1 kudos

Segger J-Link STM32H755 CM4 debugging in STM32CubeIDE

I am trying to debug the STM32H755 within CUBEIDE but the current segger J-link drivers say that core is not supported. The segger website lists it as supported and it works without issues in their debuggers.I am wondering if there is a workaround or...

Ckerl.2 by Associate II
  • 2320 Views
  • 4 replies
  • 0 kudos

Ubuntu 22.04 CubeIDE either freezing or no IOC editor

I was having this problem https://community.st.com/t5/stm32cubeide-mcus/stm32cubeide-user-interface-freezing-in-ubuntu-22-04-wayland/td-p/656993 so I tried the solution and it fixed the freezing, but now the IOC editor doesn't render, such as with ht...

DShekter by Associate III
  • 2280 Views
  • 5 replies
  • 1 kudos

STM32CubeIDE 1.14.1 Login to myST does nothing

With STM32CubeIDE 1.14.1 running on Windows10 the login to myST does not work anymore. Clicking the menu item or using the hotkey Alt-L simply does nothing - no reaction, no error message, NOTHING. It worked some time ago but all of a sudden does not...

MSchm.1 by Associate II
  • 8494 Views
  • 17 replies
  • 3 kudos

Is there support for github copilot?

Hi,I cannot find any information about the possibility to use github copilot in the STM32CubeIDE. Is it available or are there any plans to support it in the future?Or do you recommend using it in VS only?Thanks you for your answer

Hueli.1 by Associate III
  • 11931 Views
  • 7 replies
  • 12 kudos

STM32F439ZI TCP COMMUNICATION

I am a beginner in ethernet TCP protocol. I wanted to establish tcp connection between host and target(stm32f439zi). I don't know how to find ip address of an ethernet port connected in stm32.Can anyone help me to learn from basics and develop code a...

arun27 by Associate II
  • 1149 Views
  • 2 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.