STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1703 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 638 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

UChar.h is missing

Hi,I just found out <uchar.h> is missing from standard c header files in \STM32CubeIDE\plugins\com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.12.3.rel1.win32_1.1.0.202410251130\tools\arm-none-eabi\include. How am I supposed therefore to u...

GMeur by Senior II
  • 2484 Views
  • 4 replies
  • 1 kudos

Resolved! Problem opening a project CubeIDE

Win 10, x64, STM32CubeIDE version 1.17.0I'm trying to open a CubeIDE project from a workspace but it just doesn't load, see image below. I select the folder for my workspace, click finish & am then told that there are no projects in the folder. Yet t...

Cube_Proj_Issue.png

Resolved! stuck on creating a new project from ioc file

I'm trying to create a new project from a exiting ioc file.When I click the "finish" button, it shows a progress bar but disappear very fast, and it did nothing else. No new project created, no nothing. I don't know what went wrong. Is there an error...

soapshepard_0-1739770170418.png

Tips for debugging programs with CubeIDE

Please listen to the trouble and cause when debugging with CubeIDE that I was troubled withThe cause is very simple once you understand it, but I couldn't think of it at the time of trouble. Details of the trouble A CubeIDE sample program was execute...

Kiyama by Associate II
  • 1349 Views
  • 0 replies
  • 1 kudos

Resolved! "main.c" is not visible.

"main.c" is not visible.This is the screen I want.  However, this is my actual screen. I am sure I have chosen the board correctly.

image02.png image01.png
hjjang by Associate II
  • 2448 Views
  • 7 replies
  • 4 kudos

STM32H755 CM4's HAL_Delay() never returns

Hi All,I have a problem on H755 Nucleo which is that the M4's tick doesn't seem to be advancing.Digging a little deeper I can see that uwTickFreq is zero, but I can't see why that's happened. There must be something wrong in my .ioc file since I've h...

bramble by Senior
  • 1927 Views
  • 5 replies
  • 0 kudos

Resolved! Generating .srec file from command line

Hey,I am using the STM32f769NIH controller and my application has Touchgfx and freeRTOS enabled. The code downloading time is too slow and I want to speed it up.I figured that turning off the external loaders in the debug configurations yields a smal...

CubeIDE problems

Hi boys and girls from ST,I am testing your CubeIDE and it it catastrophe.1/ I tried to open a new project in CubeID and I ascertained that I can not add assembly file (s). How I can create project with only one file - in assembly. :)2/ I tried to cl...

JerryMC22 by Associate III
  • 4074 Views
  • 4 replies
  • 3 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.