2025-02-04 11:46 PM - edited 2025-02-05 2:28 AM
I'm using STM323H755ZIT6 NUCLEO board, STM32CubeMX 6.13.0 and STM32CubeIDE 1.17.0.
In my scenario, I created a project in STM32CubeMX 6.13.0 and generated the project. After that, I opened this project in STM32CubeIDE 1.17.0 and added paths for external folders in Paths and Symbols. Later, I edited the .IOC file in STM32CubeMX and tried to regenerate the project, but an error popup appeared.
ERROR POPUP
After this popup, I clicked the OK button, and STM32CubeMX showed 'Project Successfully Generated.' However, when I tried to build the project in STM32CubeIDE, it failed to build, and errors appeared, such as:
D:/NAVANEETHAN/CoffeeMaker/DisplayControl/Project/DisplayControl/CM7/Core/Src/main.c:116: undefined reference to `HAL_Init'
D:/NAVANEETHAN/InstalledSoftwares/STM32CubeIDE_1.17.0/STM32CubeIDE/plugins/com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.12.3.rel1.win32_1.1.0.202410251130/tools/bin/../lib/gcc/arm-none-eabi/12.3.1/../../../../arm-none-eabi/bin/ld.exe:
A total of 40 errors were shown, all related to HAL and OS kernel functions.
I attached All errors in Errors.txt and IOC file
anyone support about this issue
Thank you
Solved! Go to Solution.
2025-02-13 8:28 PM - edited 2025-02-13 8:32 PM
The file ..\STM32CubeIDE\.project needs to be removed. Reopening the project in STM32CubeMX and regenerating the code will resolve the mentioned issue.
2025-02-13 8:28 PM - edited 2025-02-13 8:32 PM
The file ..\STM32CubeIDE\.project needs to be removed. Reopening the project in STM32CubeMX and regenerating the code will resolve the mentioned issue.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.