STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1703 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 638 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Interactive (readline) Debug Console on macos

Using STM32CubeIDE on macos (with STM32H7431VITx, FWIW), the Debug Console has a pretty poor interface, where there's no readline support and even basic things like "arrow up" to recall the latest  command doesn't work, rather it moves the cursor up ...

haleecaero1_0-1777059782867.png

Change which programer IDE picks

I want to change /opt/st/stm32cubeide_2.0.0/plugins/com.st.stm32cube.ide.mcu.externaltools.cubeprogrammer.linux64_2.2.300.202508131133/tools/bin/STM32_Programmer_CLIto/opt/st/stm32cubeide_1.4.0/plugins/com.st.stm32cube.ide.mcu.externaltools.cubeprogr...

USBCPD SNK not generating file

HiI am trying to setup the NUCLEO-G491RE along with a X-NUCLEO-SNK1M1 to communicate with a USBC PD source.I have tried to follow the STM32StepByStep - Getting started with USB-Power Delivery Sink.STM32StepByStep:Getting started with USB-Power Delive...

LINSS by Associate
  • 204 Views
  • 1 replies
  • 0 kudos

Resolved! Project importation not working with STM32CubeIDE v1.9.0

Hello,I was working with STM32CubeIDE version 1.8.0 on a project. I just download version 1.9.0, trying to import the project.In the importation Wizard, when selecting the correct directory, the project name is displayed, but when clicking "Finish", ...

ANauz.1 by Senior II
  • 6804 Views
  • 4 replies
  • 6 kudos

Resolved! STM32CubeIDE how to show hints when calling function

Hello,STM32CubeIDE.Is it possible to show hints (description of the function, description of the parameters of the function, description of the return value) when calling function?I made this function (see Figure 1) and made documenting comment. When...

Mykola_Levun_0-1725009010067.png
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.