STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1703 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 638 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

CubeIDE: show version of the IDE

Dear ST Team,I use multiple versions of CubeIDE and would appreciate it if the currently running IDE version could be displayed in the following screens (somewhere).Thank youLike its done in GfxDesigner  

cubeIDE version 0.png cubeIDE version 1.png cubeIDE version 2.png ferro_1-1777656051778.png
ferro by Lead
  • 692 Views
  • 13 replies
  • 8 kudos

Resolved! Can't download STM32CubeIDE

Hello all,I can't download the STM32CubeIDE even as I am registered. There seems to be somthing broken with the Web page. I have tried several browsers. This is what I get, so there is no download button and the table is garbled:Any help appreciated....

eble_0-1703151708265.png
eble by Associate
  • 34291 Views
  • 35 replies
  • 26 kudos

Resolved! Is it possible to create a compile_commands.json file?

I work in a workspace but I use vim with clangd for editing my code. I am wondering if it is possible to create a compile_commands.json file and if so how. If the IDE uses cmake under the hood then it should be rather straightforward but I cannot und...

ubaldot by Senior
  • 10523 Views
  • 8 replies
  • 5 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.