STM32 MPUs Software development tools

Ask questions and find answers on STM32 microprocessors software development tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 504 Views
  • 0 replies
  • 0 kudos

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 392 Views
  • 0 replies
  • 0 kudos

STM32CubeProgrammer v2.22 released

We are pleased to announce that STM32CubeProgrammer 2.22 is available What is new in 2.22: Support for the STM32U3 microcontrollers with 2 Mbytes of flash memory: Internal memory programming through debug and bootloader interfacesOption bytes program...

Glitch in CubeMX RISAF

Dear all I was setting up the RISAF4 for STM32MP257, however, the partition with name "linuxkernel2" has a glitch where its size shows as givenWhich is beyond the size of my LDDR4 set to 8Gb.How to solve it? A quick reply will be appreciated.Thanking...

glitch.png
Amit_RS by Associate III
  • 433 Views
  • 5 replies
  • 3 kudos

A suspected bug i CubeMX for MP257

Hi!I think a have found a bug in CubeMX for STM32MP257F processor.If you go to RIF - RISAB - VDERAM. You will find that the region size can only be 0x21000. That's more than 128 kB, according to the data sheet.SYSRAM1, SYSRAM2, SRAM1, SRAM2, RETRAM h...

DMårt by Lead
  • 388 Views
  • 5 replies
  • 1 kudos

STM32MP257F-DK vs STM32MP157F-DK2

Hello,I have some sort of experience working with linux on RPI.I wanted to increase my embedded linux experience with STM32MP.So I wonder, should I buy STM32MP2 because its newer, or STM32MP1 because it will probably have more support and more refere...

onass by Associate III
  • 398 Views
  • 5 replies
  • 0 kudos

SEGGER RTT VIEWER向STM32MP257D_M33发数据有5秒以上的响应延迟

经我这三两天的多次调试,我终于找到了问题所在先说segger rtt viewer的工作方式首先,我将segger rtt的源码编译烧录到stm32mp257d_m33那里去。这时m33核的暂存会持有一个_segger_rtt结构体。然后我将这个结构体地址提供给segger rtt viewer,这时就会成功建立起通讯现在我通过segger rtt viewer向stm32mp257d_m33发送数据,这时jlink这个硬件工具就会通过swd直接操作暂存将数据写入到_segger_rtt结构体的...

csvir by Associate
  • 260 Views
  • 1 replies
  • 0 kudos

STM32MP2Dev Rust updates

I was excited to see the Rust support for the Developer Package (seen here and here)However, I am having some issues with the fact that the provided toolchain is version 1.75 rustc and cargo. Mostly the fact that this version cannot use dependencies ...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.