cancel
Showing results for 
Search instead for 
Did you mean: 

A suspected bug i CubeMX for MP257

DMårt
Lead

Hi!

I think a have found a bug in CubeMX for STM32MP257F processor.

If you go to RIF - RISAB - VDERAM. You will find that the region size can only be 0x21000. That's more than 128 kB, according to the data sheet.

SYSRAM1, SYSRAM2, SRAM1, SRAM2, RETRAM have 0x20000 as maximum region size.

Question: If this is a bug, then I want to send a PR to the Github ST repository of the MP2 firmware. Can you guide me where the code is so I can make a PR?

STM32MP151AAC3 custom board with STM32-OS as operating system: https://github.com/DanielMartensson/STM32-Computer

STM32MP257FAK3 custom board with STM64-OS as operating system: https://github.com/DanielMartensson/STM64-Computer
5 REPLIES 5
Souhaib MAZHOUD
ST Employee

Hello @DMårt 

Thank you for highlighting this issue on STCommunity.
I will check it internally with the dedicated team and get back to you as soon as possible.

BR, Souhaib

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

@Souhaib MAZHOUD

Thank you for your reply.

Waiting for the feedback.

STM32MP151AAC3 custom board with STM32-OS as operating system: https://github.com/DanielMartensson/STM32-Computer

STM32MP257FAK3 custom board with STM64-OS as operating system: https://github.com/DanielMartensson/STM64-Computer

@Souhaib MAZHOUD 

There is also issues with the field linuxkernel2 region size.

 

STM32MP151AAC3 custom board with STM32-OS as operating system: https://github.com/DanielMartensson/STM32-Computer

STM32MP257FAK3 custom board with STM64-OS as operating system: https://github.com/DanielMartensson/STM64-Computer
Souhaib MAZHOUD
ST Employee

Hello @DMårt 

An internal ticket has been raised to the dedicated team to review this issueInternal ticket number: CDM0061992 (This is an internal tracking number and is not accessible or usable by customers.)

Regarding the "field linuxkernel2 region size" could you clarify further?

BR, Souhaib

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

@Souhaib MAZHOUD 

Unfortunately, my laptop having some issues. So, I cannot show you what I mean. But according what's happening is that the field linuxkernel2 having some issues. It's not possible to configure. Check the values of the start and region size.

STM32MP151AAC3 custom board with STM32-OS as operating system: https://github.com/DanielMartensson/STM32-Computer

STM32MP257FAK3 custom board with STM64-OS as operating system: https://github.com/DanielMartensson/STM64-Computer
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.