2026-03-12 7:34 AM
It's telling me (for example) there's a "Path Entry Problem":
Invalid project path: Include path not found (C:\Users\xxx\Documents\xxx\USB_CDC\USB_Device\Target).The Tool Settings / MCU GCC Compiler / Include paths contains
"${workspace_loc:/${ProjName}/Application/USB_Device/Target}"and in my project there is a folder Application/USB_Device/Target, it links to a folder
C:\Users\xxx\Documents\xxx\USB_CDC\STM32CubeIDE\Application\USB_Device\TargetHow can I figure out where this warning is coming from?
(notice - the project builds just fine, it's just a warning, but company policy is to build without warnings)
2026-03-12 7:48 AM - edited 2026-03-12 7:52 AM
@cbcooper wrote:The Tool Settings / MCU GCC Compiler / Include paths contains
Note that there are also Include Paths under other tools (eg, Assembler), and under C/C++ General.
Also check in other Configurations.
@cbcooper wrote:How can I figure out where this warning is coming from?
I agree that Eclipse (on which CubeIDE is built) is unhelpful here.
@cbcooper wrote:company policy is to build without warnings
Note that this is an IDE warning, not a compiler warning
PS:
As CubeIDE is Eclipse, a general search for "Eclipse Path Entry Problem" might help; eg,
2026-03-12 8:20 AM
As far as I can tell, the values in "Properties / C/C++ General / Paths and Symbols" are just a re-telling of the information I put in "C/C++ Build / Settings / Tool Settings / MCU GCC Compiler / Include paths".
I've checked both Release and Debug configurations.
The question you linked to on stackoverflow says to remove "$YOUR-PROJECT.sc" from "$WORKSPACE/.metadata/.plugins/org.eclipse.cdt.make.core" but for me that folder only contains specs.c and specs.cpp and they are both empty.
I do see there are lots of questions about Eclipse generating Path Entry Problems and I've tried several without success, they are all just workarounds anyway (delete files, close project, turn around three times, open project while closing left eye). I'm assuming it's some kind of interaction between Eclipse and STM32CubeIDE and that both parties are assuming it's the other one's fault.
2026-03-12 8:51 AM
@cbcooper wrote:some kind of interaction between Eclipse and STM32CubeIDE and that both parties are assuming it's the other one's fault.
STM32CubeIDE is Eclipse.
Have you tried doing an Index rebuild?
(it's in the pop-up when you right-click the Project in the Project Explorer).
Otherwise I guess it's a case of deleting each Include Path entry until you find it ...
2026-03-19 11:17 AM
@Andrew Neil wrote:Note that there are also Include Paths under other tools (eg, Assembler), and under C/C++ General.
@cbcooper I've just had this very problem occur and it was, indeed, caused by entries in the Assembler Include Paths.
It seems that the paths had been added to both Compiler and Assembler at some point.
Have you checked that?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.