2025-12-11 8:48 AM - edited 2025-12-17 10:26 PM
This post provides a workaround for a specific issue in STM32CubeIDE v2.0.0. The issue will be resolved in the next version.
If STM32CubeIDE v2.0.0 is installed from scratch and if the imported project in STM32CubeIDE v2.0.0 is a project generated with STM32CubeMX v6.16, it is not possible to install the OpenSTLinux plugin. Consequently, it is not possible to import OSTL projects such as Linux, Optee, TF-A, or U-Boot.
In order to work around this, the following steps are recommended:
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.