STM32 MPUs Products and hardware related

Ask questions and find answers on STM32 microprocessors, including hardware, power, DRAM, flashing, interfacing, device tree, and peripherals.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

On VMWare's Ubuntu 20.04 LTS, the STM32 program tool is not associated with the STM32MP157D evaluation board.

Hello, teachers.​First, The board I am using is the STM32MP157D evaluation board.​I checked the article that the starter package can be installed in Windowsos, but the developer package and the distribution package are only available in the Linux env...

kKim.1 by Associate II
  • 3355 Views
  • 3 replies
  • 0 kudos

having trouble in configuring device tree for STM32MP157c based board by karo-electronics, QSMP1570 on qsbase2, having yocto kirkstone and kernel 5.15, where to find the macros to be used in dts files, because i am unable to bitbake after my change

I have a board from karo-electronics, STM32MP157c based QSMP 1570 SOM over qsbase2, I am trying to configure above mentioned board for my specific application, The distribution is build using yocto by karo-electronics, I am unable to edit the dts fil...

SChat.2 by Associate II
  • 3161 Views
  • 4 replies
  • 0 kudos

Resolved! Can I install the developer package on the STM32MP157D-EV1 board using "Windows os" STM32Cubeprogrammer program?

I even installed the starter package in EMMC boot mode.And I want to install a developer package.I want to install SDK, can I use STM32MP157D-EV1 board using STM32Cube Programmer in Windows OS?Ubuntu 18.04 was installed in virtualbox and STM32Cubepro...

kKim.1 by Associate II
  • 1579 Views
  • 1 replies
  • 0 kudos

Resolved! Install Ubuntu 18.04 (LTS) on STM32MP157D-EV1 board with starter package installed

I am using the STM32MP157D-EV1 board.The starter package is currently installed in EMMC boot mode.the version is "ST OpenSTLinux - Weston - (A Yocto Project Based Distro) 4.0.4-openstlinux-5.15-yocto-kirkstone-mp1-v22.11.23 \n \l" .I need to install ...

kKim.1 by Associate II
  • 1562 Views
  • 1 replies
  • 0 kudos

STM32MP1 FDCAN issues

Hello,I have the stm32mp157c-dk2 board and have connected two CAN Bus transceivers to it.FDCAN1 is assigned to the A7 CPU and the FDCAN2 is assigned to the M4 CPU.Both transmitters are connected to the same CAN bus. There is also a 3rd device connect...

Artem by Associate III
  • 15109 Views
  • 22 replies
  • 0 kudos

Start M4 firmware automatically

Hi!I am using STM32MP157C-DK2 and i want to start the coprocessor from bootloader (I have readed the wiki page). First, I have done it manually and everithing works fine:I have changed kernel m4_rproc:&m4_rproc{ /*Restriction: "memory-region" proper...

JIrao.1 by Associate
  • 2782 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.