2023-01-31 9:58 PM
I am using the STM32MP157D-EV1 board.
The starter package is currently installed in EMMC boot mode.
the version is "ST OpenSTLinux - Weston - (A Yocto Project Based Distro) 4.0.4-openstlinux-5.15-yocto-kirkstone-mp1-v22.11.23 \n \l" .
I need to install Ubuntu 18.04 on this board, but I don't know how.
Do I have to delete the installed package now and install Ubuntu 18.04?
Ah, I downloaded the ubuntu-18.04.6-desktop-amd64.iso file.
I can use Windows 10 and Oracle virtualbox.
I want to use Windows 10 if possible, but if it's impossible, I can also use Oracle virtualbox.
Solved! Go to Solution.
2023-02-02 1:32 AM
Hi @kKim.1 ,
"I need to install Ubuntu 18.04 on this board"
This is not possible!
It looks like you mixed you PC / Host machine setup requiring Ubuntu 20.04 LTS and the STM32MP157D-EV1 target board which can only support the provided OpenSTLinux distribution.
Can you clarify ?
Olivier
2023-02-02 1:32 AM
Hi @kKim.1 ,
"I need to install Ubuntu 18.04 on this board"
This is not possible!
It looks like you mixed you PC / Host machine setup requiring Ubuntu 20.04 LTS and the STM32MP157D-EV1 target board which can only support the provided OpenSTLinux distribution.
Can you clarify ?
Olivier
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.