STM32 MPUs Products and hardware related

Ask questions and find answers on STM32 microprocessors, including hardware, power, DRAM, flashing, interfacing, device tree, and peripherals.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Start M4 firmware from A7 application

Hi!I am using STM32MP157C-DK2 board to create an application on the screen (using GTK library). My idea is to start coprocessor firmware from the A7 application with the following commands (system commands):int main (int argc, char **argv) { GtkApp...

0693W00000Y92TKQAZ.png
TArre.1 by Associate III
  • 4583 Views
  • 6 replies
  • 1 kudos

How to convert init manager from sysvinit to systemd and run weston at startup in yocto project?

Using yocto project and changed default sysvinit to systemd with below line in local.confINIT_MANAGER = "systemd" DISTRO_FEATURES += "pam vulkan opengl egl wayland" CORE_IMAGE_EXTRA_INSTALL += "wayland weston" IMAGE_INSTALL:append = " chromium-ozone-...

Seenu by Associate II
  • 2705 Views
  • 1 replies
  • 0 kudos

STM32MP157C-DK2 flash didn't work.

I've tried to flash STM32MP157C-DK2 SDCard like described in ST wiki with command STM32_Programmer_CLI -c port=usb1 -w flashlayout_st-image-weston/FlashLayout_sdcard_stm32mp157c-dk2-trusted.tsv.and it didn't work! i got following error report. it see...

RYin by Associate II
  • 9492 Views
  • 15 replies
  • 0 kudos

Resolved! Upgrade STM32MP157C-EV1 to STM32MP157F-EV1

I have a STM32MP157C-EV1 board.Can i upgrade STM32MP157C-EV1 board to STM32MP157F-EV1 only removing TM32MP157C processor and reinstaling a new TM32MP157F processor?If not, how can i upgrade MB1263 MPU subsystem daughterboard to the last microprocesso...

JSaav.1 by Associate
  • 1819 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.