2023-02-01 9:20 PM
I even installed the starter package in EMMC boot mode.
And I want to install a developer package.
I want to install SDK, can I use STM32MP157D-EV1 board using STM32Cube Programmer in Windows OS?
Ubuntu 18.04 was installed in virtualbox and STM32Cubeprogrammer was installed. However, the program cannot read the STM32 board on the USB port.
I want to install Ubuntu 18.04 on the STM32MP157D-EV1 board. Is there any way?
Solved! Go to Solution.
2023-02-02 1:36 AM
Hi @kKim.1 ,
There's no way to install Ubuntu 18.04 or SDK on the target board STM32MP157D-EV1.
It looks like you mixed Host / PCs requirement and ecosystem side and the target side.
On Host side : Ubuntu 20.04 LTS on which you can install developper package (SDK + source code) or Distribution ( Yocto)
Target side : Only support OpenSTLinux executable binaries cross-compiled on you PCs thanks to Developper or Distribution package and download with STM32CubeProg on your boot device (eMMC, SDCard et.. )
Hope it help,
Olivier
2023-02-02 1:36 AM
Hi @kKim.1 ,
There's no way to install Ubuntu 18.04 or SDK on the target board STM32MP157D-EV1.
It looks like you mixed Host / PCs requirement and ecosystem side and the target side.
On Host side : Ubuntu 20.04 LTS on which you can install developper package (SDK + source code) or Distribution ( Yocto)
Target side : Only support OpenSTLinux executable binaries cross-compiled on you PCs thanks to Developper or Distribution package and download with STM32CubeProg on your boot device (eMMC, SDCard et.. )
Hope it help,
Olivier
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.