2020-12-17 6:46 AM
Hello, I'm using STM32WB55 for my application and I'm following the AN5289 Rev 3 to write data into flash. When the BLE is looking for a device to connect, the procedure stuks checking PESD bit for more then 30 seconds. It is normal?
I suppose the amount of time the program is stuck is directly connected to the timeout of the "searching" phase. Is it true?
If I jump that control, the procedure fails, so, do you have any suggestion to follow?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.