2026-03-29 11:22 PM - last edited on 2026-03-30 2:39 AM by Andrew Neil
Hi Team,
We are observing persistent and repeatable debug connectivity issues on multiple custom boards based on the STM32H745BIT6 MCU. These boards were initially functioning as expected; however, after repeated debug sessions, they started exhibiting failures. We request your support in identifying the potential root causes and guidance on recovery. We have performed Full Chip erase also whenever it was possible.
Below are our consolidated observations captured across multiple boards.
Debug Interface Failures After Multiple Sessions
After several debug sessions, the following errors are observed intermittently:
Inconsistent Connectivity Between Tools
Loss of Debug Connection During Runtime
Target is not responding, retrying...
Temporary Recovery After Power Cycle
STMicroelectronics ST-LINK GDB server. Version 7.11.0
Copyright (c) 2025, STMicroelectronics. All rights reserved.
Starting server with the following options:
Persistent Mode : Disabled
Logging Level : 1
Listen Port Number : 61234
Status Refresh Delay : 15s
Verbose Mode : Disabled
SWD Debug : Enabled
InitWhile : Enabled
Waiting for debugger connection...
Target is not responding, retrying...
Target is not responding, retrying...
Target is not responding, retrying...
Target is not responding, retrying...
Debugger connected
Target is not responding, retrying...
Target is not responding, retrying...
Target is not responding, retrying...
Target is not responding, retrying...
Target is not responding, retrying...
Target is not responding, retrying...
Target is not responding, retrying...
Target is not responding, retrying...
Target is not responding, retrying...
Target is not responding, retrying...
Target is not responding, retrying...
Target is not responding, retrying...
Target is not responding, retrying...
Target is not responding, retrying...
Target is not responding, retrying...
Target is not responding, retrying...
Session manager. Fail starting session.
GDB server. Fail create session.
Waiting for debugger connection...
Shutting down...
Exit.
STMicroelectronics ST-LINK GDB server. Version 7.11.0
Copyright (c) 2025, STMicroelectronics. All rights reserved.
Starting server with the following options:
Persistent Mode : Disabled
Logging Level : 1
Listen Port Number : 61234
Status Refresh Delay : 15s
Verbose Mode : Disabled
SWD Debug : Enabled
InitWhile : Enabled
Target no device found
Error in initializing ST-LINK device.
Reason: No device found on target.
10:21:00 : UR connection mode is defined with the HWrst reset mode
10:21:00 : ST-LINK SN : 004A00303234510537333934
10:21:00 : ST-LINK FW : V3J16M9B5S1
10:21:00 : Board : STLINK-V3SET
10:21:00 : Voltage : 3.30V
10:21:00 : Error: No STM32 target found! If your product embeds Debug Authentication, please perform a discovery using Debug Authentication
10:21:10 : UR connection mode is defined with the HWrst reset mode
10:21:10 : ST-LINK SN : 004A00303234510537333934
10:21:10 : ST-LINK FW : V3J16M9B5S1
10:21:10 : Board : STLINK-V3SET
10:21:10 : Voltage : 3.29V
10:21:10 : SWD freq : 8000 KHz
10:21:10 : Connect mode: Normal
10:21:10 : Reset mode : Core reset
10:21:10 : Device ID : 0x450
10:21:10 : Revision ID : Rev V
10:21:10 : Debug in Low Power mode is not supported for this device.
10:21:11 : UPLOADING OPTION BYTES DATA ...
10:21:11 : Bank : 0x00
10:21:11 : Address : 0x5200201c
10:21:11 : Size : 308 Bytes
10:21:11 : UPLOADING ...
10:21:11 : Size : 1024 Bytes
10:21:11 : Address : 0x8000000
10:21:11 : Read progress:
10:21:11 : Data read successfully
10:21:11 : Time elapsed during the read operation is: 00:00:00.004
10:21:18 : UPLOADING ...
10:21:18 : Size : 1024 Bytes
10:21:18 : Address : 0x8100000
10:21:18 : Read progress:
10:21:18 : Data read successfully
10:21:18 : Time elapsed during the read operation is: 00:00:00.003
10:21:47 : Error: Unable to get core ID
10:21:47 : Error: Unable to get core ID
10:21:47 : Error: Unable to get core ID
10:21:47 : Warning: Connection to device 0x450 is lost
10:21:48 : Disconnected from device.
10:53:37 : UR connection mode is defined with the HWrst reset mode
10:53:37 : ST-LINK SN : 004A00303234510537333934
10:53:37 : ST-LINK FW : V3J16M9B5S1
10:53:37 : Board : STLINK-V3SET
10:53:37 : Voltage : 3.30V
10:53:37 : SWD freq : 8000 KHz
10:53:37 : Connect mode: Normal
10:53:37 : Reset mode : Core reset
10:53:37 : Device ID : 0x450
10:53:37 : Revision ID : Rev V
10:53:37 : Debug in Low Power mode is not supported for this device.
10:53:38 : UPLOADING OPTION BYTES DATA ...
10:53:38 : Bank : 0x00
10:53:38 : Address : 0x5200201c
10:53:38 : Size : 308 Bytes
10:53:38 : UPLOADING ...
10:53:38 : Size : 1024 Bytes
10:53:38 : Address : 0x8100000
10:53:38 : Read progress:
10:53:38 : Data read successfully
10:53:38 : Time elapsed during the read operation is: 00:00:00.003
10:54:14 : Error: Unable to get core ID
10:54:14 : Error: Unable to get core ID
10:54:14 : Error: Unable to get core ID
10:54:14 : Warning: Connection to device 0x450 is lost
10:54:15 : Disconnected from device.
10:55:02 : UR connection mode is defined with the HWrst reset mode
10:55:04 : ST-LINK SN : 004A00303234510537333934
10:55:04 : ST-LINK FW : V3J16M9B5S1
10:55:04 : Board : STLINK-V3SET
10:55:04 : Voltage : 3.30V
10:55:04 : Error: ST-LINK error (DEV_TARGET_NOT_HALTED)
10:56:03 : UR connection mode is defined with the HWrst reset mode
10:56:03 : ST-LINK SN : 004A00303234510537333934
10:56:03 : ST-LINK FW : V3J16M9B5S1
10:56:03 : Board : STLINK-V3SET
10:56:03 : Voltage : 3.30V
10:56:03 : Error: No STM32 target found! If your product embeds Debug Authentication, please perform a discovery using Debug Authentication
Based on the above behavior, we would appreciate your help with:
Identifying possible root causes.
Looking forward to your guidance on restoring the affected devices to a stable and debuggable state.
Best regards,
M S Kavya
Solved! Go to Solution.
2026-03-30 1:07 AM
Hello,
It could be a hardware issue.
Please review your schematics based on the AN4938 "Getting started with STM32H74xI/G and STM32H75xI/G MCU hardware development", especially VCAP capacitors, the decoupling capacitors.
It could be also a soldering joint issue.
2026-03-30 1:07 AM
Hello,
It could be a hardware issue.
Please review your schematics based on the AN4938 "Getting started with STM32H74xI/G and STM32H75xI/G MCU hardware development", especially VCAP capacitors, the decoupling capacitors.
It could be also a soldering joint issue.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.