STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 301 Views
  • 1 replies
  • 2 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4118 Views
  • 0 replies
  • 3 kudos

HELP - CMWX1ZZABZ-078 project on STM32CubeIDE

Hello everyone, I'm trying to compile together a project Created with STM32CubeIDE based on STM32L082 and STM32CubeExpansion_LRWAN_V1.3.1 but I'd like to keep it configurable through CubeMX.Is there someone that succeded in this? There are a lot of f...

AComa.170 by Associate II
  • 1936 Views
  • 2 replies
  • 0 kudos

I'm trying to implement custom callbacks on the STM32WB Zigbee library. Any examples of custom callbacks on a report or certain attributes?

My goal is to have a coordinator connected to sleepy end devices. The coordinator will periodically request measurements from the end devices. It seems like all the examples have requests going from the nodes to the coordinator, so I'm having trouble...

MCope.1 by Associate II
  • 2910 Views
  • 4 replies
  • 0 kudos

Resolved! STM32WB55 : Using event process functions tables.

Hi.In SDK I foud interesting source files: ble_events.h, ble_events.c, in wich we have 3 structures defined as hci_event_table_t.Also in ble_legacy.h we have a defines to that structures.Every strucrure have event code and callback and callback calls...

Resolved! nucleo-wb55 virtualCOMPort error

Hello everyone,I'm trying to create a BLE project as virtualCOMPort to start and after saving the setup wizard, when it compiles I get an undefined reference to `MX_BlueNRG_MS_Init and MX_BlueNRG_MS_Process'.This functions are declared inside 'app_b...

JSanz.1 by Associate III
  • 4358 Views
  • 6 replies
  • 0 kudos

MAC 802.15.4 Stack CubeMX configuration

Hello,Currently start working on MAC 802.15.4 application on STM32WB. Quick question - should I configure this stack through CubeMX, or should I copy it from CubeWB package manually and set the respective #define? Because, currently in STM32_WPAN sec...

DBogd.1 by Associate
  • 785 Views
  • 0 replies
  • 0 kudos

Resolved! Problems with project generated by CubeMX (Keil , STM32WB55)

Hello! I have a project where I set up the BLE , then I decided to add FreeRTOS to this project. But the problem is that there is an error in the generated project that I cannot solve (It seems the error is from Cube).(...).axf: Error: L6200E: Symbol...

0693W000004HLhpQAG.png 0693W000004HLhuQAG.png
Kolab by Senior
  • 3149 Views
  • 8 replies
  • 0 kudos

Resolved! I want to output modulated and unmodulated waves in order to receive radio wave certification. How can I output them?

HelloI have to obtain radio wave certification for products using STM32WB50. Is it possible to output modulated and unmodulated waves with STM CubeMonRF?The protocol stack we are using is MAC_802_15_4_FFD.bin. I can't understand it even if I call it ...

MNitt.1 by Associate II
  • 1557 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.