2025-06-05 6:24 AM - last edited on 2025-06-05 6:27 AM by Andrew Neil
After performing an OTA update, the Bluetooth icon appears as shown in Figure 1, but it does not display the "STM_OTA" name.The correct result should look like Figure 2.
I followed the modification steps from this video, including adding the OTA Reboot Characteristic as shown:
https://www.youtube.com/watch?v=mRzZOa3jmuM&list=PLnMKNibPkDnG9JRe2fbOOpVpWY7E4WbJ-&index=9https://www.youtube.com/watch?v=mRzZOa3jmuM&list=PLnMKNibPkDnG9JRe2fbOOpVpWY7E4WbJ-&index=9
The chip I’m using is STM32WB55CGU6, with FUS version v2.0, and ST BLE Toolbox version 1.4.4.
The project has been uploaded in the attachment.
Solved! Go to Solution.
2025-06-06 5:25 AM
2025-06-05 6:29 AM
2025-06-05 6:31 AM
Is this the same question:
2025-06-05 6:35 AM
This is not the same issue. This is a new problem. Currently, OTA updates can be successful, but it can only be updated once and cannot be updated again.
2025-06-05 6:39 AM
So is the previous one now resolved?
If so, please mark the solution in that thread.
2025-06-05 6:42 AM
The previous issue has been resolved, but how should this new problem be addressed?
2025-06-06 5:25 AM
2025-06-06 6:20 AM
Hello,
please read this document carefully.
Also, I recommend having a look at BLE_HeartRate_ota example which can be helpful as a reference project.
Best regards,
Filip Kremen
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.