STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 301 Views
  • 1 replies
  • 2 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4118 Views
  • 0 replies
  • 3 kudos

WBA: Seed errors on RNG

Hi,I have one board where, depending on PLL configuration, it yields a lot of seed errors on RNGThis is the faulty configuration RCC_OscInitStruct.PLL1.PLLSource = RCC_PLLSOURCE_HSI; RCC_OscInitStruct.PLL1.PLLFractional = 0; RC...

STM32WL FUOTA Firmware swapping issue

Hello everyone, The LoRaWAN_End_Node from LoRaWAN_FUOTA Project (STM32Cube_FW_WL_V1.3.1) is used with ChirpStack as a network server (supports the FUOTA Package V1).  The Multicast session runs and receives the Downlink of all the Fragmented Packets ...

AElgh_0-1749025843655.png AElgh_2-1749026679942.png AElgh_1-1749026569602.png
AElgh by Associate III
  • 1428 Views
  • 3 replies
  • 0 kudos

nucleo-stm32wl55jc-fuotav1

Good morning allIm trying to follow the https://github.com/actility/nucleo-stm32wl55jc-fuotav1?tab=readme-ov-file#readme in order to simulate a firmware update on my STM32WLJC1 nucleo board but i am running into a something strange.  All the projects...

HKhan.4 by Associate II
  • 779 Views
  • 0 replies
  • 0 kudos

Resolved! STM32WB15 Using LPUART instead of USART1

Hello,I am currently using the NUCLEO-WB15CC to test STM32CubeMonitor-RF.I imported the BLE_TransparentMode example to be able to use Monitor RF. Everything works perfectly when using the default USART1 interface.I also tested the communication using...

Midleware_TransparentMode_Configuration.png

Resolved! X-NUCLEO-67W61M1 Pack, support for STM32F401/F411

I expect to re4ceive my 67W61M1 expansion board very soon. However, in looking at the CubeMX pack for the device I do not see a driver for STM32F4xx devices. Is this planned or are we on our own porting using the Pack examples?

SidPrice by Associate III
  • 1559 Views
  • 2 replies
  • 1 kudos

STM32WB5 BLE UART Not Working

Dear Sirs, I have been developing an Application that runs in the STM32WB5 for a while, the BLE works fine, and it is integrated with a mobile app fine, but I need to communicate it with a coprocessor (STM32H750). For this mean, I would like to use U...

VCasa3_0-1748439898563.png VCasa3_1-1748439920395.png VCasa3_2-1748439939283.png
VCasa.3 by Associate II
  • 1370 Views
  • 3 replies
  • 0 kudos

Resolved! USBX on STM32WBA6

Hello,On CubeMX v6.14.1 and X-CUBE-AZRTOS-WB v6.2.0, I am not able to add a USB record/playback device. This means that I cannot generate USB Device descriptors using CubeMX. Why is this not possible yet? What are the alternatives?Best regards,Navin 

NRedd2_0-1747468885037.png
NRedd.2 by Senior
  • 4182 Views
  • 10 replies
  • 3 kudos

STM32WLE5

Is the DevEUI ID also provided in the hardware for stm32wle , in datasheet it is mentioned it is DevEUI compliant. Does it also have a UID64 register from where it can be read? 

LGEOR.1 by Associate II
  • 1904 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.