STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 301 Views
  • 1 replies
  • 2 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4118 Views
  • 0 replies
  • 3 kudos

Resolved! cant program FUS and stack.

Hi.I'm working with the EVAL STM32WB5MM-DK for a while now, already programmed the stack and the FUS many times, and it's the first time I got this error.After successfully open STM32CubeProgrammer (v2.19) and connected to the programmer, Selecting t...

netanelu_0-1750019098157.png netanelu_1-1750019210318.png
netanelu by Associate III
  • 1108 Views
  • 2 replies
  • 0 kudos

Resolved! Unable to turn on BLE WAPN on extended-full stack

Hey there,i have a custom board designed which is broadcasting stuff over BLE.So far i am using the full_stack_fw which works quite well.In order to turn on extended advertising i wanted to switch over to the full_extended_stack (needed for extended ...

Exeu_0-1750413452410.png Exeu_1-1750413528054.png
Exeu by Associate III
  • 1512 Views
  • 4 replies
  • 1 kudos

pROBLEM WITH stm32WB05KZ wake-up proccess

Hi, I'm having a problem with the wake-up procces using interruptions. I use three pins, PA0, PA8 and PA9, set the with no pull-up, and in rising mode. then i enable them as wake up pins, in rising mode. i go to sleep in stop mode, using the function...

LuisL by Associate
  • 804 Views
  • 1 replies
  • 0 kudos

Systick Interrupt issue

Hello Team,I am currently working on STM32WLE5 microcontroller and getting issue in HAL_Delay(), it got stuck, ifound that systick interrupt was not generating. In main() function, I start with HAL_Init() and then HAL_Delay(500) and controller get st...

Ronik_123 by Associate II
  • 2984 Views
  • 9 replies
  • 3 kudos

Resolved! LC3 CODEC transparent mode.

Hi,I was going through the documentation in this link. It mentions that there is a transparent mode. How can I enable this in the example for PBP Source?/* Codec Mode */ typedef uint8_t CODEC_Mode_t; #define CODEC_MODE_DEFAULT (CODEC_MODE_FLOW_C...

NRedd.2 by Senior
  • 2457 Views
  • 8 replies
  • 0 kudos

Resolved! It is possible to set two vector table in same flash

I am implementing a dual-firmware architecture on an STM32 microcontroller that does not natively support dual-bank flash. In this setup, I have partitioned the internal flash memory into two separate blocks:Block 1 (Bootloader + Application) begins ...

jackiee by Associate
  • 909 Views
  • 1 replies
  • 1 kudos

Resolved! SHUTDOWN mode WUP Pin works but no WUF is set at wakeup

I've a custom board that going to SHUTDOWN OFF mode I'm using the LPM lib and it use PA0 as WAKEUP PIN it wakes up on a High level signal void PWR_EnterOffMode(void) { /* USER CODE BEGIN PWR_EnterOffMode_1 */ // refer to the following link for more...

oga by Associate III
  • 1121 Views
  • 3 replies
  • 1 kudos

Resolved! Problem with flash in stm32wb55

Hello.I found a problem with Flash. After successfully operating with flash before entering MX_APPE_Process(), the possibility of entering standby mode disappears. I had issues with the visibility of variable values after these operations, but I coul...

IlliaGx by Senior
  • 3494 Views
  • 10 replies
  • 4 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.