2025-06-17 1:56 AM - last edited on 2025-06-17 5:28 AM by Andrew Neil
in stm32wb55, After generating p2p configuration, #include "ble_types.h" should add manually in p2p_stm32.h file.
Solved! Go to Solution.
2025-06-17 10:22 AM - edited 2025-06-17 10:24 AM
Hello @nima.askari
I've personally generated a code on the STM32WB using the STM32_WPAN and the P2P server application type. After compilation, everything works fine and no need to add the file manually (using the STM32CubeMX V6.14.1 and the STM32CubeIDE V1.18.1). If you have the need to use the ble_types.h and it is not included, you need to ad it manually.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2025-06-17 5:28 AM
Is that a question, or a statement?
2025-06-17 10:22 AM - edited 2025-06-17 10:24 AM
Hello @nima.askari
I've personally generated a code on the STM32WB using the STM32_WPAN and the P2P server application type. After compilation, everything works fine and no need to add the file manually (using the STM32CubeMX V6.14.1 and the STM32CubeIDE V1.18.1). If you have the need to use the ble_types.h and it is not included, you need to ad it manually.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.