NUCLEO-WBA25CE1 "Bootloader limitation"
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link MATTER - Matter software expansion for STM32Cube - STMicroelectronics It is a reference implementation for the demonstration of Matter on ST...
Please go and visit our wiki pages where you can find a lot of information on our wireless product families (WB, WBA, WL) and the supported protocols: BLE, Zigbee, Thread, Matter, Lora, ... To begin your technical journey, please start from this top ...
Posted on March 23, 2018 at 20:00 Hi, I've made a custom board based on CMWX1ZZABZ-091 which contains theSTM32L072CZ device and am currently trying to modify existing End_Node (\STM32CubeExpansion_LRWAN_V1.1.4\Projects\Multi\Applications\LoR...
Posted on June 21, 2018 at 11:22Hello,I'm new to LoRa network, and I would like to use the B-L072Z-LRWAN1 board to exchange data with a server. I use the I-CUBE-LRWAN 'Ping Pong' project as a starting point. I'd like to modify the ping pong app to e...
Posted on June 08, 2018 at 05:21Hi,I'm actually working with a LoRaWAN kit (https://techship.com/products/acsip-lorawan-evk-antenna-kit-s76sxb/) based on STM32L073x and Semtech SX1276 radio module.So the kit comes with examples based on Semtech exam...
Posted on June 14, 2018 at 22:58Having a problem with ST-Link v2-1 programming the STM32CubeExpansion_LRWAN boards.Have updated the firmware and using the latest driver for WIndows 10.Programming requires constant driver restarting. Debugging from t...
Posted on June 14, 2018 at 18:54Hello,i see that in the CUBE for lorawan, the HAL_InitTick function has been rewritten, with a simple return and does nothing, replacing the standard in the HAL_drivers, so the timeout function of every other HAL don'...
Posted on June 12, 2018 at 17:39Hi,I am working on a project about LoRa expansion board, I have an stm32l053 Nucleo and an I-NUCLEO-LRWAN1 with a sx1272 transceiver.I am trying to compile the PING PONG project from STM32CubeExpansion_LRWAN_V1.1.5, b...
Posted on June 12, 2018 at 15:35Hello We were looking for controller which provides BLE feature in it. We came across STM32WB55VG ARM controller which as BLE 5.0. We have few quarry regarding it, they are:1. We could not find much details about BLE ...
Posted on April 27, 2017 at 11:23The CalculateBackOff method of teh i cuve lrwan is too old and contains a major bug for join duty cycle procedure.The calcBackOff.ElapsedTime is always now !.In case of a new Initiliazation of the LoRa Stack, maybe 1...
Posted on January 02, 2018 at 14:09My team and I are currently working on a project that involve a ST board (the STM32L072CZYxx) to create a bidirectionnal GSM-LoRa gateway.As we've already succeeded in implementing the GSM side of the gateway, we a...
Posted on June 01, 2018 at 06:19Hi,I am having problems with downloading I-CUBE_LRWAN project onto the B-L072Z-LRWAN1 development module.The error message I am receiving is 'internal command error'. I am also having the same connection problem with ...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.