2018-06-12 8:39 AM
Hi,
I am working on a project about LoRa expansion board, I have an stm32l053 Nucleo and an I-NUCLEO-LRWAN1 with a sx1272 transceiver.
I am trying to compile the PING PONG project from STM32CubeExpansion_LRWAN_V1.1.5, but each time there is RX_TIMEOUT that appears on the terminal (termite or terra term or even Putty). And we have no communication between our 2 modules. We tried do make some modifications, such as those shown in the link below:
We also tried to run the code and verify that there is a transmission with a spectrum analyzer, but nothing appeared.
We were trying to understand the functioning of the ping-pong example to understand how the transmission with LoRa Module works. Because our target is to enable communication between 2 LoRa module, one as a master (its mission will be to collect the data of the different sensors and transmit it,) and the other one as a slave (its mission is to receive the data of the master and then transmit it with Uart to the PC).
If you may want help us to find a solution to our problem.
Thank you.
#lorawan #lora #ping-pong #i-nucleo-lrwan1 #sx1272 #stm32l0532018-06-13 6:41 AM
Last time I worked on this was with LRWAN_v1.1.1, but ported to the USI module, and demonstrated rx and tx operation. The Ping-Pong example is a rather pointless and unstable application, I ported point-to-point demo code I built for the DISCO and Multi-Tech boards.
>>If you may want help us to find a solution to our problem.
For commercial work I'm open to reasonable offers for my time.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.