2018-05-31 9:19 PM
Hi,
I am having problems with downloading I-CUBE_LRWAN project onto the B-L072Z-LRWAN1 development module.
The error message I am receiving is 'internal command error'.
I am also having the same connection problem with st-link utility. However, I am able to update the firmware with ST-LinkUpgrade.
I have tried removing and leaving the CN8 jumpers along with having CN11 connected.
Cheers,
Andrew
#lorawan #keil-ide #keil #b-l072z-lrwan12018-05-31 10:53 PM
Define LOW_POWER_DISABLE so it doesn't turn off the debug interface and drop connectivity. Stuff doesn't work well without power and clocks.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.