NUCLEO-WBA25CE1 "Bootloader limitation"
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link MATTER - Matter software expansion for STM32Cube - STMicroelectronics It is a reference implementation for the demonstration of Matter on ST...
Please go and visit our wiki pages where you can find a lot of information on our wireless product families (WB, WBA, WL) and the supported protocols: BLE, Zigbee, Thread, Matter, Lora, ... To begin your technical journey, please start from this top ...
Hi All,Seeking some information regarding whether there will be any future releases of FW supporting a dual stack for the Murata CMWX1ZZABZ-078 module for both LoRa and SigFox in parallel.Are there any announcements for supporting this feature in the...
As I said in the title, I tried to test the PingPong example avaliable in the I-CUBE-LRWAN software expansion but it does not work on B-L072Z-LRWAN1 board.After importing the project to SW4STM32 and running it (without doing any modifications), this ...
I am fairly new to STM32 programming and I want to stablish a communication between both boards (B-L072Z-LRWAN1 and NUCLEO-L053R8 + I-NUCLEO-LRWAN1). I was wondering if I can achieve this goal using the PingPong example located in the Cube expansion ...
Posted on July 03, 2018 at 14:10 Hello , I use this demo board B-L072Z-LRWAN1 with the soft End Node I-CUBE-LRWAN But I don’t understand why I can’t send the data once when I want with function send() or LORA_send() in the main or in the whi...
Posted on July 11, 2018 at 15:17Hello,until now i have a serial connection to my Board. So i just have to read out my COM Port to get the Data i need. My next step is to get rid of the cable. Which Module would you recommend for this? And is it much...
Posted on July 16, 2018 at 11:25Hello,I am trying to update from firmware 2.6 to 3.7 (following the document https://github.com/USIWP1Module/USI_I-NUCLEO-LRWAN1/blob/master/preloaded_firmware/WM-SG-SM-42%20Update%20Preloaded%20AT%20Command%20FW%20Ap...
Posted on June 05, 2018 at 09:24Hi everyone,I'm working on B-L072Z-LRWAN1 lora discovery kit and i have an issue.I'm able to upload my program on STM32 and it run when the STM is plug in on USB STLINK.My issue is when i want run my STM on 3AAA batte...
Posted on June 19, 2018 at 15:16Hello everyone,I have a discovery board B-L072Z-LRWAN1 running the End Node LoRa application provided in the I-CUBE-LRWAN package.My problem is the next :- The join procedure works well.txDonerxDoneJOINED- But when a ...
Posted on January 19, 2018 at 17:25Hello.I was working with the LRWAN software using the Murata module a couple of months ago and was happy with its operation and functionality on my custom PCB. I moved over to hardware/antenna development and now h...
Posted on June 27, 2018 at 18:24Hello,I don't understand what is the purpose of the STSAFE_nRST pin. Could you please explain to me ?Thanks in advance.Best Regards,Malo#stsafe #cmwx1zzabz
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.