STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 301 Views
  • 1 replies
  • 2 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4118 Views
  • 0 replies
  • 3 kudos

STM32L476RG + IDW01M1 - WiFi hangs before connecting

Posted on May 28, 2018 at 22:41Hi! I'm looking for some help in getting my STM32L476RG and IDW01M1 up and running with the FP-CLD-AZURE1 STM32Cube function pack. I also have the sensors.I've flashed the board with the relevant binaries etc... The Az...

Programming STM32L0 board in B-L072Z-LRWAN1

Posted on May 23, 2018 at 09:03I have been working on stm32 lora discovery kit B-L072Z-LRWAN1 board and what i want to do is, I want to program the STM32L0 board and access all the other pis related to it. The peripherals mentioned and given in the ...

Use of X-NUCLEO-LPM01A with STM32L072

Posted on May 22, 2018 at 12:32Hello everyone, This is my first post here.As part of my research with LoRaWAN, I am working on a custom built board having an STM32L072 module. One of the critical sections of my research involves calculating the ener...

STM32L0 Timer 2 CH1 not triggering interrupt

Posted on May 11, 2018 at 10:33HiI am using B-L072Z-LRWAN STM32 Eval board for configuring sensor.The sensor gives PWM as output.To measure the width I am using GPIOA 5 (PA5) pin as Timer input.I am using the following code for Timer configuration:&...

SigFox stack for B-l072Z-LRWAN1

Posted on May 08, 2018 at 10:04Hi, I have some trouble getting the sigfox stack up and running on B-l072Z-LRWAN1 kit together with SDR Dongle from Sigfox, what i have done so far is:1. Executed SignatureGenerator.bin on my device and retrieved the s...

B-L072Z-LRWAN1 is not recognize (COM port)

Posted on April 27, 2018 at 14:57Dear Community,I've bought 2 different evaluation boards to know better LoRa with STM32 MCUs. First, I bought the Nucleo board with the Mbed shied from Semtech ( P-NUCLEO-LRWAN1). I've managed to connect it to my lap...

STM32L072CZ Lora Keil License

Posted on May 04, 2018 at 13:54Hi,if I build the programm 'AT-Slave' (STMCubeExpansion_LRWAN) I got an License Error from Keil ( error: L6050U: The code size of this image (38072 bytes) exceeds the maximum allowed for this version of the linker.). I...

B-L072Z-LRWAN1 CN11 (USB Conn.) - Device mode

Posted on May 01, 2018 at 16:05Hi Everyone,I would like to ask a question regarding to powering the B-L072Z-LRWAN1 direct from the CN11 USB connector.The user manual of the B-L072Z-LRWAN1 states the following:''When the B-L072Z-LRWAN1 board is power...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.