STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 301 Views
  • 1 replies
  • 2 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4118 Views
  • 0 replies
  • 3 kudos

STM32 Kit with high accuracy crystal

Hi,I am looking for an STM based MCU/kit with high accuracy crystal oscillator with possible option to fine tune the frequency. I want to use it for some high accuracy time reference. Looking for suggestion please.- ijaz

IAhma.1 by Associate II
  • 6031 Views
  • 13 replies
  • 0 kudos

Resolved! STM32WB - STM32Cube SAI HAL code generation bug

Hi,I found a possible bug in the "stm32wbxx_hal_msp.c" file when using Cube in the STM32CubeIDE to enable the SAI peripheral.I did not test all the combinations, but have mine set up as follows:SAI A - Async SlaveSAI B - Sync Slave The bug is that th...

0693W00000D0ERXQA3.jpg
DeonT by Associate
  • 2414 Views
  • 4 replies
  • 1 kudos

FOTA STM32WB not restart with many android phones

I am using BLE OTA bootloader found in CubeWb1.8.0 to upload a firmware to a custom STM32WB55CG device. I am using ST BLE sensor app to upload the firmware from an android phone to the custom device. I was able to successfully carry out FOTA and rest...

ASiva.1 by Associate III
  • 1276 Views
  • 1 replies
  • 0 kudos

STM32WB55 Medical Applications

Hello,I wanted to know is there any product in the market where STM32 MCUs are used in Implantable Devices. Are there any Medical Norms for STM Controllers? Can we Use STM32WB as a Implantable with BLE?Thanks in Advance.

STM32WL with HSE and XTAL

I am trying to start HSE with external crystal (on nucleo WL55JC1 board). I removed R2 (Output from TCXO), added two 0E bridges R39 and R40, added 10k resistor R41 (to remove stub). Then I started the Cube-MX (latest, fresh update...), selected the n...

0693W00000D15ucQAB.jpg
s54mtb by Associate II
  • 3347 Views
  • 3 replies
  • 0 kudos

Is it multi-regional application possible?

Hi, everyone. Is it possible to build an application that supports all regional standards? AS923-1 / AS923-2 / AS923-3 together are of particular interest (depending on the setting, which is changed via the UART, for example).

OSole.1 by Associate II
  • 1411 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.