STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 301 Views
  • 1 replies
  • 2 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4118 Views
  • 0 replies
  • 3 kudos

Sources for ST BLE Sensor 4.12.0

Hello dear tech support and comunity.Is it possible to get sources for ST BLE Sensor 4.12.0 for Android and were?Here https://github.com/STMicroelectronics/STBlueMS_Android it seems to be only 4.9.0 as latest one.BRAlex

Shum47 by Associate
  • 873 Views
  • 0 replies
  • 0 kudos

Resolved! How to stop the example program getting recovered ?

when the example file is modified but the original program gets recovered when the Device Configuration Tool Code Generation is hit after some changes in ioc file.#stm32wl55jcIts hard to start from the scratch in LoRa subghz, Do anyone have some meth...

SSaya.1 by Associate II
  • 1003 Views
  • 2 replies
  • 0 kudos

Hello, STM32WB55 Power Consumption measurement with STM32 Nucleo Expansion Board which has Microcontroller STM32L496.

I am Attaching Observed Current Consumptions. I am observing Huge Difference between claimed current value versus observed current value at various low power modes. I am having right Connections as mentioned in Power Consumption measurement board Dat...

Resolved! Firmware release v1.12.0 breaks BLE and Flash erase behavior

Hello,There's a degradation in flash erase during BLE connection use-case between release 1.11.1 and 1.12.0.On 1.12.0 flash erase operation will cause the BLE client to disconnect (timeout).Same user code just the different FW version - 1.11.1 works,...

APort by Associate III
  • 1109 Views
  • 2 replies
  • 0 kudos

I'm working on P-NUCLEO-LRWAN3 as a mistake i delete every data from NUCLEO-L073RZ, now i have no idea how to comunicate with the sensor shield.

On the site of Rising hf i found a solution: "STM32Nucleo_ATCmd_Bridge-v0.1.3-20170920.bin". This file is impossible to find online. I tryed a usb- serial comunication with the sensor shield, but i can only recive data and not sending them. The lora...

Carbone_M by Associate II
  • 2293 Views
  • 4 replies
  • 0 kudos

STM32WL55 LoRaWAN EndNode Application I2C stop2 doesn't work.

i am trying to implement I2C for the LPS33HW Sensor in the LoraWAN endnode application. I know that the STM32WL55JC in the IDLE Mode it is going into the STOP2 Mode. Therefore i defined the i2c3 because it can be woken up without a lose. The Clock fo...

0693W00000D1o2VQAR.png 0693W00000D1o2QQAR.png 0693W00000D1o2LQAR.png 0693W00000D1o2GQAR.png
PNeub.2 by Associate II
  • 1160 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.