NUCLEO-WBA25CE1 "Bootloader limitation"
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link MATTER - Matter software expansion for STM32Cube - STMicroelectronics It is a reference implementation for the demonstration of Matter on ST...
Please go and visit our wiki pages where you can find a lot of information on our wireless product families (WB, WBA, WL) and the supported protocols: BLE, Zigbee, Thread, Matter, Lora, ... To begin your technical journey, please start from this top ...
Hello guys,I am using STM32WB and also get stuck when I try to enable hci_le_advertising_report_event()I use examble BLE_MeshLightingRFL and in function Ble_Hci_Gap_Gatt_Init(), I command function aci_gap_create_connection() at the endIt return BLE_S...
Hello?Likes title, I want to ask for writing method using ST-Link(SWD, 4000 kHz).Problem is error at erasing stage. "Error : FUS_STATE_ERR_UNKNOWN"(Version of STM32CubeProgrammer is 2.5.0, result of this UI also same.)And, result of reading addre...
I am using STM32L152RET6 running I-CUBE-LRWAN V1.2.1 CLASS A. I am pushing data to TTN and I can perfectly see the uplinks and downlinks from my LoRaWAN Gateway (RHF0M301):JSON up: {"rxpk":[{"tmst":56541636,"chan":2,"rfch":0,"freq":915.500000,"stat":...
I'trying STN32WLcube firmware 1.1.0. The LoRaWAN End Node works as aspected and now I need to add my sensors, but when I debug it I have the error "Target is not responding, retrying..."DEBUGGER_ENABLED value is set to 1 ( I think is the same as DEBU...
TLDR; The current tools for BLE in STM32CubeIDE and STM32CubeMX do not work properly for custom BLE profiles in the STM32WB55. When will the tools support it, and when will the documentation be updated with the current system?Firstly, I would prefer ...
Hi, I am new to STM32.I am trying to implement LoRa Receiver and Transmitter code in STM32WL. I have tried to modify the Rx and Tx code using the Ping-Pong application code (subghz_phy_app.c) . I have added my Transmitter code below, can you please r...
Hi everyone, I am trying to read ADC values from 4 different channels PC0 ------> ADC1_IN1 PC1 ------> ADC1_IN2 PC2 ------> ADC1_IN3 PC3 ------> ADC1_IN4I am able to get different values from different channel for the 1st iteration. but from th...
I need to connect in such a way that Arduino read sensors data and pass them to the Lorawan board that will transmit to the Gateway
According to the subject, I found I can't enter to the stop2 mode ,when i run the ble stack (APPE_Init() ) in p2p_server. I tried to use HAL_PWREx_EnterSTOP2Mode(PWR_STOPENTRY_WFI); behind the aci_gap_set_non_discoverable(); but it wasn't wor...
When attempting to add an accelerometer to the LoRaWAN_End_Node program, on the SPI1 interface, I find that it works (in polled mode) until the board sleeps and is woken with an interrupt. Then the SPI1 Control Register 1 and Control Register 2 are c...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.