2021-02-21 9:41 AM
Hi,
I am new to STM32.
I am trying to implement LoRa Receiver and Transmitter code in STM32WL. I have tried to modify the Rx and Tx code using the Ping-Pong application code (subghz_phy_app.c) .
I have added my Transmitter code below, can you please review the code and suggest changes.
Also, how can I change the time duration of messages sent by the transmitter end node?
Rgds,
Frank
/* Includes ------------------------------------------------------------------*/
#include "platform.h"
#include "stm32_timer.h"
#include "sys_app.h"
#include "subghz_phy_app.h"
#include "radio.h"
#include "stm32_seq.h"
#include "utilities_def.h"
#include "app_version.h"
uint16_t BufferSize = BUFFER_SIZE;
uint8_t Buffer[BUFFER_SIZE];
int8_t RssiValue = 0;
int8_t SnrValue = 0;
/* Led Timers objects*/
static UTIL_TIMER_Object_t timerLed;
/* Radio events function pointer */
static RadioEvents_t RadioEvents;
/* Private function prototypes -----------------------------------------------*/
/*!
* @brief Function executed on when led timer elapses
* @param LED context
* @retval none
*/
static void OnledEvent(void *context);
/*!
* @brief Function to be executed on Radio Tx Done event
* @param none
* @retval none
*/
static void OnTxDone(void);
/*!
* @brief Function executed on Radio Tx Timeout event
* @param none
* @retval none
*/
static void OnTxTimeout(void);
/* Exported functions ---------------------------------------------------------*/
void SubghzApp_Init(void)
{
/* Led Timers*/
UTIL_TIMER_Create(&timerLed, 0xFFFFFFFFU, UTIL_TIMER_ONESHOT, OnledEvent, NULL);
UTIL_TIMER_SetPeriod(&timerLed, LED_PERIOD_MS);
UTIL_TIMER_Start(&timerLed);
/* Radio initialization */
RadioEvents.TxDone = OnTxDone;
RadioEvents.TxTimeout = OnTxTimeout;
Radio.Init(&RadioEvents);
Radio.SetTxConfig(MODEM_LORA, TX_OUTPUT_POWER, 0, LORA_BANDWIDTH,
LORA_SPREADING_FACTOR, LORA_CODINGRATE,
LORA_PREAMBLE_LENGTH, LORA_FIX_LENGTH_PAYLOAD_ON,
true, 0, 0, LORA_IQ_INVERSION_ON, TX_TIMEOUT_VALUE);
Radio.SetMaxPayloadLength(MODEM_LORA, BUFFER_SIZE);
Radio.SetChannel(RF_FREQUENCY);
APP_LOG(TS_ON, VLEVEL_L, "Tx start\n\r");
Radio.Send(Buffer, BufferSize);
#if defined(USE_BSP_DRIVER)
BSP_LED_Init(LED_GREEN);
BSP_LED_Init(LED_RED);
#elif defined(MX_BOARD_PSEUDODRIVER)
SYS_LED_Init(SYS_LED_GREEN);
SYS_LED_Init(SYS_LED_RED);
#else
#error user to provide its board code or to call his board driver functions
#endif /* USE_BSP_DRIVER || MX_NUCLEO_WL55JC*/
}
/* Private functions ---------------------------------------------------------*/
static void OnTxDone(void)
{
/* USER CODE BEGIN OnTxDone_1 */
/* USER CODE END OnTxDone_1 */
APP_LOG(TS_ON, VLEVEL_L, "OnTxDone\n\r");
Radio.Sleep();
UTIL_SEQ_SetTask((1 << CFG_SEQ_Task_PingPong_Process), CFG_SEQ_Prio_0);
/* USER CODE BEGIN OnTxDone_2 */
/* USER CODE END OnTxDone_2 */
}
static void OnTxTimeout(void)
{
/* USER CODE BEGIN OnTxTimeout_1 */
/* USER CODE END OnTxTimeout_1 */
APP_LOG(TS_ON, VLEVEL_L, "OnTxTimeout\n\r");
Radio.Sleep();
State = TX_TIMEOUT;
UTIL_SEQ_SetTask((1 << CFG_SEQ_Task_PingPong_Process), CFG_SEQ_Prio_0);
/* USER CODE BEGIN OnTxTimeout_2 */
/* USER CODE END OnTxTimeout_2 */
}
static void OnledEvent(void *context)
{
/* USER CODE BEGIN OnledEvent_1 */
/* USER CODE END OnledEvent_1 */
#if defined(USE_BSP_DRIVER)
BSP_LED_Toggle(LED_GREEN) ;
BSP_LED_Toggle(LED_RED) ;
#elif defined(MX_BOARD_PSEUDODRIVER)
SYS_LED_Toggle(SYS_LED_RED) ;
SYS_LED_Toggle(SYS_LED_GREEN) ;
#endif /* USE_BSP_DRIVER || MX_BOARD_PSEUDODRIVER */
UTIL_TIMER_Start(&timerLed);
/* USER CODE BEGIN OnledEvent_2 */
/* USER CODE END OnledEvent_2 */
}
/* USER CODE BEGIN PrFD */
/* USER CODE END PrFD */
/************************ (C) COPYRIGHT STMicroelectronics *****END OF FILE****/
2021-05-17 4:36 AM
Hi,
1/you need to register the task in SubghzApp_Init function
/*register task to to be run in while(1) after Radio IT*/
UTIL_SEQ_RegTask((1 << CFG_SEQ_Task_SubGHz_Phy_App_Process), UTIL_SEQ_RFU, PingPong_Process);
2/
then you should implement the function PingPong_Process with what you want to do next. (start a timer to trigger the next Radio.Send?)
Best Regards,
2021-08-15 11:43 PM
hello, is it possible to send UART data by modifying the ping pong payload?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.