2020-09-10 9:53 AM
Hello?
Likes title, I want to ask for writing method using ST-Link(SWD, 4000 kHz).
Problem is error at erasing stage. "Error : FUS_STATE_ERR_UNKNOWN"
(Version of STM32CubeProgrammer is 2.5.0, result of this UI also same.)
And, result of reading address '0x20030030' is 00000000.
Source is modified from Remi QUINTIN's(ST Employee) batch file in below link.
https://community.st.com/s/profile/0050X000007vjlkQAA
I'm using STM32WB5xxE(512K), address of FUS_fw is 0x0807A000(ver 1.0.2) and address of Stack_fw is 0x08057000(ver 1.3.1).
Apart from the above, CPU1(application code) seems to have no problem in operation.
Please review command sources.
Thank you.
S. Y. Lee
--------------------------------------------------------------------------------------------------
@echo off
SET PROG="C:\Program Files\STMicroelectronics\STM32Cube\STM32CubeProgrammer\bin\STM32_Programmer_CLI.exe"
SET BIN_PATH=C:\Users\PC\STM32Cube\Repository\STM32Cube_FW_WB_V1.3.0\Projects\STM32WB_Copro_Wireless_Binaries\
SET APPLI_PATH=C:\Atollic\TEST_BLE1\Debug\
set comport=SWD
echo Connected with %comport%
REM Command list
SET S0=%PROG% -c port=%comport% -rdu
SET DOWNLOAD=%PROG%
REM FW list
SET RF_STACK_BIN=%BIN_PATH%stm32wb5x_BLE_Stack_fw.bin
SET FUS_BIN=%BIN_PATH%stm32wb5x_FUS_fw.bin
REM SET APPLI=%APPLI_PATH%TEST_BLE1.hex
REM list the port com
%PROG% -l
echo REMOVE read Out protection
REM This command removes the memory Read protection by changing the RDP level from level 1 to 0
%PROG% -c port=swd -rdu
echo read Out protection removed
echo current FUS version
%PROG% -c port=swd -r32 0x20030030 1
echo mode HOTPLUG
%PROG% -c port=swd mode=HOTPLUG -r32 0x20030030 1
REM Delete the RF stack located in the secure area.
REM The goal is to let more space for the donwload of the new FUS
echo delete RF stack
%PROG% -c port=SWD -fwdelete
REM FUS/Stack upgrade via Debug (STLINK) Interface :
echo FUS Upgrade :
%PROG% -c port=swd mode=UR -ob nSWboot0=0 nboot1=1 nboot0=1 -fwupgrade %FUS_BIN% 0x0807a000 firstinstall=1
timeout 5
echo new FUS version
%PROG% -c port=swd -r32 0x20030030 1
Stack install :
echo RF stack installation
%PROG% -c port=swd mode=UR -ob nSWboot0=0 nboot1=1 nboot0=1 -fwupgrade %RF_STACK_BIN% 0x08057000
timeout 3
REM User application install :
echo application programming
%PROG% -c port=swd mode=UR -d %APPLI% 0x08000000 -v
REM All these operations can be combined in one command :
%PROG% -c port=swd mode=UR -ob nSWboot0=0 nboot1=1 nboot0=1 -fwupgrade %FUS_BIN% 0x0807a000 firstinstall=1 -c port=swd mode=UR -fwupgrade %RF_STACK_BIN% 0x08057000 -c port=swd mode=UR -d %APPLI% 0x08000000 -v
echo RESET Board/button
pause
2020-10-14 6:03 AM
CLI.exe -c port=swd -r32 0x20030030 1 does not work for SWD port as the device information table is not located at this address when the SWD port is used for programming.
I assume a few lines have been uncommented, especially the last one with all the commands sent at once, which is absolutely useless if the previous commands were used.
Moreover the FUs should be loaded only once with the same version otherwise you may face some errors.
So please use the latest CubeWB FWacakge v1.9.
Then could you download the option byte to understand what is the current status of your chip.
2021-08-09 10:35 PM
Hi SLee,
did you finally manage to program your board? It looks like I'm facing the same issue but couldn't fix it yet.
Best Regards
Markus
2021-08-17 5:28 AM
No, I didn't.
I don't know what is problem.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.