2021-08-15 6:47 AM
I need to connect in such a way that Arduino read sensors data and pass them to the Lorawan board that will transmit to the Gateway
2021-08-15 7:07 AM
The B-L072Z-LRWAN1 can interface with shields directly.
To communicate with a secondary processing board you'll probably want to use UART connectivity.
The D0/D1 pins would provide such an interface, so you'll need to use these and a GND pin.
Download a schematic and user manual for the board, and review those.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.