NUCLEO-WBA25CE1 "Bootloader limitation"
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link MATTER - Matter software expansion for STM32Cube - STMicroelectronics It is a reference implementation for the demonstration of Matter on ST...
Please go and visit our wiki pages where you can find a lot of information on our wireless product families (WB, WBA, WL) and the supported protocols: BLE, Zigbee, Thread, Matter, Lora, ... To begin your technical journey, please start from this top ...
Note: I can use stlink to download programs to other boards.But p_nulceo_wb55 doesn't work well. I use an external stlink instead of the on-board stlink, the errors are same.I was learning Bluetooth, It would have worked well. After a while, an erro...
Brief: I am using cubemx to configure and generate code.MCU: stm32wb55rgvxfirmware package name and version: FW_WB V1.13.3Details:I am working on a project where the stm must act as a bridge between the PC and the device under test (DUT). We use the ...
I'm trying to use the STM32WB firmware event callbacks defined in ble_events.h and ble_events.c but they don't appear to be working.According to the documentation in PM0271 revision 2 section 4.4 I should be able to use the event callbacks framework ...
Hello,I have a project which contains both: Bootloader (BL) and Application (App.)The BL is based on minimal devices without interrupts, mainly RS485 - and worked Fine!The App. is based on "BLE_PERIPHERAL_LITE" example by ST, with my additional freeR...
This device isn't connecting with the network that I have plan of connectivity LoRaWAN.When I open the serial connection I see that the information is being read as it should. However, the connection to the network it's just not working at all. I use...
I make a pcb board with stm32wb55rgv6, but my LSE doesn't work and this part of the circuit was accidentally destroyed in my soldering process. Can i just use HSE or LSI in replace of LSE in BLE application? And what's the limitations?
i modified the code for downlink turning on red led 3." case LORAWAN_USER_APP_PORT:"for my case port 99:to turn on led defined at PB1 which i defined.as this was the default code for digital output given by cayenne port 99.when i am gpio writing whe...
Hi,Am currently running optical character reading in NUCLEO-WL55JC2 with camera attached. I want to send the reading data to the Lora Dashboard. I connected another similar board for lora and sent the received data to lora and then to dashboard. I...
I chose Lora E5 Mini to get a sensor measurement. For my application, I do not need a gateway and connection to a server like thingspeak. I want to make two end devices communicate. I configured the device in ABP mode, set the Tx and Rx frequency and...
Hello,I am having a problem with my P-NucleoWB55 development board. When using STMCUBEIDE and trying to debug, I get the following error.Failed to start GDB serverError in initializing ST-LINK device.Reason: (4) No device found on target.I also cann...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.