NUCLEO-WBA25CE1 "Bootloader limitation"
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link MATTER - Matter software expansion for STM32Cube - STMicroelectronics It is a reference implementation for the demonstration of Matter on ST...
Please go and visit our wiki pages where you can find a lot of information on our wireless product families (WB, WBA, WL) and the supported protocols: BLE, Zigbee, Thread, Matter, Lora, ... To begin your technical journey, please start from this top ...
Hi all, I want to do some tests to simulate "low coverage" conditions How could I quickly make the equipment transmit at less power? For example in the EU868 region limit to 10dBm instead of the 14dBm that is allowed, or in US915 to 20dBmn inst...
Hello every body,I got stuck in Flash programming of STM32WB55CEU MCU!!! and I can not find the problem.First. I implemented the stm32wb55 example FLASH_EreaseProgram on Nucleo board successfully and then I tried to port this simple program on my PCB...
Hello!I need to consider the best BLE stack firmware for production and its release provided by STMicroelectronics.Is there some long term version or some release that have long term support status?Are there some plans in BLE stack firmware developme...
Hello,I am using STM32WLE5CC for my project of Lorawan FUOTA Project. I wanted to do FUOTA task with my application, but I think, there would be issue of size. According to FUOTA document, Firmware max size is 84kB, and When I compile only Generated ...
I''m working on STM32WL55 series microcontroller and I want to use KEIL IDE,Please let me know does keil support STM32WL55 for FREE
Hello guys,I was inspecting the design files of the Nucleo board and could not understand the use of the capacitor used for the TCXO. In the image attached (nucelo design schematic file), a note says that the C31 is used in order to avoid stubs on XT...
Hello,So I already downloaded the Lorawan_End_Node example into my Nucleo board and I could see how it works with the TeraTerm terminal.However, now I'm trying to generate a new code from the .ioc file with the CubeMX (I only added the debugger optio...
Hi, Everyone. I have encountered a problem in using BLE with STM32WB55CG. I made custom STM32WB55CG board and the schematic is below.When I was testing the functions of the MCU, there was an abnormality in the BLE function. All other peripherals work...
HI all,I tried change option bytes for STM32WB55 in code, and probably something went wrong when I did this. After programming MCU I found that my flash was probably be blocked:How can I unblock FLASH? I tried change security config options in STM32C...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.