STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 301 Views
  • 1 replies
  • 2 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4118 Views
  • 0 replies
  • 3 kudos

CPU2 and SDK support

I already got it: CPU2 is not accessible by customer (at least, using official SDK).Anyway, we have an WB-based project that will hugely benefit from offloading some resource-consuming tasks to CPU2. They are not related to radio, we're not using any...

TwisteR by Associate II
  • 1468 Views
  • 1 replies
  • 0 kudos

Resolved! Not generating PWM signal after wake up from STOP2

I'm working with STM32WL and trying to be able to generate PWM signal after wake up from STOP2 to control RGB LED. Before going to STOP2 I deinitialize PWM channel pin and disable timer clock. MCU wakes up on button press. After wake up timer clock i...

JNowa.4 by Associate III
  • 1745 Views
  • 2 replies
  • 0 kudos

how to learn STM32 Debugger?

I had one STM32 debugger (ST-LINK-v2). how to learn the STM32 debugger and how to connect the stm32 chip to the debugger. give any solution or tutorial.I will be waiting for your replays. Thank you.

AA.21 by Associate II
  • 7679 Views
  • 20 replies
  • 0 kudos

No RX timeout IRQ after RX in single mode with timeout

If I call SUBGRF_SetRx() with a timeout of, let's say 100 ticks in LoRa mode, I don't get an RX timeout IRQ at the end of the timeout.I have checked the radio status with SUBGRF_GetStatus(). The radio goes to RX then back to standby.I have cross-chec...

HugoL by Associate II
  • 1779 Views
  • 1 replies
  • 1 kudos

Resolved! SWV not working with nucleo-wl55jc1

I'm trying to use printf with SWV.I'm using a nucleo-wl55jc1 board (stm32wl55). I have soldered SB8 to connect SWO to stlink.I have made all the config but the it doesn't show any trace.this is my setup:Create an empty STM32 project for the NUCLEO-WL...

0693W00000QLe4nQAD.png 0693W00000QLe6AQAT.png 0693W00000QLe6jQAD.png 0693W00000QLe5MQAT.png
mboua.1 by Associate
  • 1291 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.