2022-07-27 2:21 AM
I'm working with STM32WL and trying to be able to generate PWM signal after wake up from STOP2 to control RGB LED. Before going to STOP2 I deinitialize PWM channel pin and disable timer clock. MCU wakes up on button press. After wake up timer clock is beeing enabled and channel pin is reinitialized. Despite that the LED is off. What else should I do to make it work or what I've done wrong?
/* USER CODE BEGIN 2 */
GPIO_InitTypeDef GPIO_InitStruct = {0};
/* Green LED on */
HAL_TIMEx_PWMN_Start(&htim16, TIM_CHANNEL_1);
__HAL_TIM_SET_COMPARE(&htim16, TIM_CHANNEL_1, 1000);
HAL_Delay(500);
/* DeInit of LED pin, disable TIM16 clock */
HAL_TIMEx_PWMN_Stop(&htim16, TIM_CHANNEL_1);
HAL_GPIO_DeInit(LED_G_CH_GPIO_Port, LED_G_CH_Pin);
__HAL_RCC_TIM16_CLK_DISABLE();
/* Enter STOP2 */
HAL_SuspendTick();
HAL_PWREx_EnterSTOP2Mode(PWR_STOPENTRY_WFI);
/* Wake up from STOP2 on button press */
SystemClock_Config();
HAL_ResumeTick();
/* Enable TIM16 clock */
__HAL_RCC_TIM16_CLK_ENABLE();
/* ReInit of LED pin */
__HAL_RCC_GPIOB_CLK_ENABLE();
GPIO_InitStruct.Pin = LED_G_CH_Pin;
GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
GPIO_InitStruct.Pull = GPIO_NOPULL;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
GPIO_InitStruct.Alternate = GPIO_AF14_TIM16;
HAL_GPIO_Init(LED_G_CH_GPIO_Port, &GPIO_InitStruct);
/* Green LED on */
HAL_TIMEx_PWMN_Start(&htim16, TIM_CHANNEL_1);
__HAL_TIM_SET_COMPARE(&htim16, TIM_CHANNEL_1, 1000);
/* USER CODE END 2 */
Solved! Go to Solution.
2022-07-27 3:29 AM
I've removed clock disabling before going to sleep and changed procedure after wake up. The code after wake up looks like that:
/* Wake up from STOP2 on button press */
SystemClock_Config();
HAL_ResumeTick();
MX_TIM16_Init();With just MX_TIM16_Init() function everything works as expected.
2022-07-27 3:00 AM
Read out and check/compare/post content of TIM and relevant GPIO registers for working and non-working cases.
JW
2022-07-27 3:29 AM
I've removed clock disabling before going to sleep and changed procedure after wake up. The code after wake up looks like that:
/* Wake up from STOP2 on button press */
SystemClock_Config();
HAL_ResumeTick();
MX_TIM16_Init();With just MX_TIM16_Init() function everything works as expected.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.